<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC1313 Clockwire on Low</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1313-Clockwire-on-Low/m-p/528003#M752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by m.Harms on Thu May 13 03:14:41 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Helle at all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a application with the LPC 1313 and 1113. After the first programming I can´t reprogramm the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The programmer have an error request. The SWCLK pin is low when I connect the programmer to the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the application I have the reset pin set as IO Pin and disable all Pullup and Pulldown Resitors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the user manuel I have found a note that not allowed is to use the reset pin as IO pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anybody help me with this problem?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:32:53 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:32:53Z</dc:date>
    <item>
      <title>LPC1313 Clockwire on Low</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1313-Clockwire-on-Low/m-p/528003#M752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by m.Harms on Thu May 13 03:14:41 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Helle at all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a application with the LPC 1313 and 1113. After the first programming I can´t reprogramm the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The programmer have an error request. The SWCLK pin is low when I connect the programmer to the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the application I have the reset pin set as IO Pin and disable all Pullup and Pulldown Resitors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the user manuel I have found a note that not allowed is to use the reset pin as IO pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anybody help me with this problem?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1313-Clockwire-on-Low/m-p/528003#M752</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:32:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1313 Clockwire on Low</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1313-Clockwire-on-Low/m-p/528004#M753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by domen on Sat May 22 11:03:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Manually pull-up the Reset pin with ~10k resistor?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Still, I find this a bit weird, on power fail IO pin settings should reset, no?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1313-Clockwire-on-Low/m-p/528004#M753</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:32:54Z</dc:date>
    </item>
  </channel>
</rss>