<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UART after Deep Sleep Wake Up (LPC1114) in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-after-Deep-Sleep-Wake-Up-LPC1114/m-p/526597#M7</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shashankiim on Mon Jun 24 01:11:50 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey Guys&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been working with the power down modes of LPC1114 (302).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The system runs on IRC connected to PLL at the frequency of 48MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I configured a pin as wakeup source. While putting the microcontroller in deep sleep mode I power down all the oscillators and peripherals available in PDRUNCFG.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When the system wakes up by the external interrupt, the LED glows as expected however on the UART instead of the original data I get random data. Adding a delay after the wake up, gives initial characters as correct rest all as dots or garbage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Even after re configuring the UART after wake up the same issue persists. What can be the issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the correct way to wake up ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any pointers would be really appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rgds&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:34:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:34:11Z</dc:date>
    <item>
      <title>UART after Deep Sleep Wake Up (LPC1114)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-after-Deep-Sleep-Wake-Up-LPC1114/m-p/526597#M7</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shashankiim on Mon Jun 24 01:11:50 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey Guys&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been working with the power down modes of LPC1114 (302).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The system runs on IRC connected to PLL at the frequency of 48MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I configured a pin as wakeup source. While putting the microcontroller in deep sleep mode I power down all the oscillators and peripherals available in PDRUNCFG.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When the system wakes up by the external interrupt, the LED glows as expected however on the UART instead of the original data I get random data. Adding a delay after the wake up, gives initial characters as correct rest all as dots or garbage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Even after re configuring the UART after wake up the same issue persists. What can be the issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the correct way to wake up ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any pointers would be really appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rgds&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-after-Deep-Sleep-Wake-Up-LPC1114/m-p/526597#M7</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:34:11Z</dc:date>
    </item>
  </channel>
</rss>