<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debugging NXP 1769 .elf binaries in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debugging-NXP-1769-elf-binaries/m-p/540221#M6853</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by g40 on Thu May 31 06:52:59 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How do you set up an LPCXpresso project for an existing ELF binary built for the 1769? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The normal Eclipse route would be &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Import &amp;gt;&amp;gt; C/C++Executable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Select the GNU ELF parser (binary built with arm-eabi-none) and then the .elf file itself&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However there are 2 problems:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. once you hit Finish in the Import Wizard a 'Multiple problems have occurred' dialog pops up showing 'Open '%1$s' debug configuration'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. I cannot see how to tell LPCX that this is a 1769 project and it needs to fire up LPCLink and download before running GDB&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using Version: LPCXpresso v4.2.2 [Build 275] [03/04/2012]&amp;nbsp; on Windows 7 x64&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:27:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:27:58Z</dc:date>
    <item>
      <title>Debugging NXP 1769 .elf binaries</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debugging-NXP-1769-elf-binaries/m-p/540221#M6853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by g40 on Thu May 31 06:52:59 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;How do you set up an LPCXpresso project for an existing ELF binary built for the 1769? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The normal Eclipse route would be &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Import &amp;gt;&amp;gt; C/C++Executable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Select the GNU ELF parser (binary built with arm-eabi-none) and then the .elf file itself&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However there are 2 problems:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. once you hit Finish in the Import Wizard a 'Multiple problems have occurred' dialog pops up showing 'Open '%1$s' debug configuration'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. I cannot see how to tell LPCX that this is a 1769 project and it needs to fire up LPCLink and download before running GDB&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using Version: LPCXpresso v4.2.2 [Build 275] [03/04/2012]&amp;nbsp; on Windows 7 x64&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debugging-NXP-1769-elf-binaries/m-p/540221#M6853</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:27:58Z</dc:date>
    </item>
  </channel>
</rss>