<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Using static libraries in LpcXpresso v. 4 and v. 5</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539868#M6683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Nov 14 10:23:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: micronpn&lt;/STRONG&gt;&lt;BR /&gt; So the problme is that I have no liblinks.xml file in both libraries directories.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your lib directory doesn't include liblinks.xml :confused::eek::confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How did you create it ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: "Smart update" is a function, which can be used to add library settings to a project :) It's faster and easier than doing that manually (= adding path to 'Includes','Libraries' and 'Paths and Symbols'). 'Smart Update' is writing these things to Debug and Release Configuration of every selected project. Therefore 'liblinks.xml' is created in a 'C Static Library Project', which is including this information.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:17:29 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:17:29Z</dc:date>
    <item>
      <title>Using static libraries in LpcXpresso v. 4 and v. 5</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539866#M6681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micronpn on Wed Nov 14 09:57:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I just started 2 new projects both using 2 static libraries. So my workspace is organized with inside the 2 projects and the 2 libraries (all are related to the same application). I followed these instructions &lt;/SPAN&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/StaticLibrarySupportv4&lt;/A&gt;&lt;SPAN&gt; because this way should be simpler then the manual one (that also has some problems but I will write a separate post). So the problme is that I have no liblinks.xml file in both libraries directories.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any trick to use the Share function that I don't know?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539866#M6681</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using static libraries in LpcXpresso v. 4 and v. 5</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539867#M6682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micronpn on Wed Nov 14 10:00:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I made an error: my question is not about "share" but about "smart update".&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539867#M6682</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:17:29Z</dc:date>
    </item>
    <item>
      <title>Re: Using static libraries in LpcXpresso v. 4 and v. 5</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539868#M6683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Nov 14 10:23:36 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: micronpn&lt;/STRONG&gt;&lt;BR /&gt; So the problme is that I have no liblinks.xml file in both libraries directories.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your lib directory doesn't include liblinks.xml :confused::eek::confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How did you create it ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: "Smart update" is a function, which can be used to add library settings to a project :) It's faster and easier than doing that manually (= adding path to 'Includes','Libraries' and 'Paths and Symbols'). 'Smart Update' is writing these things to Debug and Release Configuration of every selected project. Therefore 'liblinks.xml' is created in a 'C Static Library Project', which is including this information.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-static-libraries-in-LpcXpresso-v-4-and-v-5/m-p/539868#M6683</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:17:29Z</dc:date>
    </item>
  </channel>
</rss>