<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 8K Limit and linker errors in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539199#M6396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cwpjr on Thu Jan 24 14:20:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Launch CR V5,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Initial Msg Box:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;License type: UNACTIVATED (Activation not completed)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Debug limit: 8k &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Activation code: not available &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Welcome screen:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]LPCXpresso5 is fully activated[/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; Welcome to LPCXpresso 5. The software is now fully activated,&amp;nbsp; and can be used for production. LPCXpresso can be used to generate and download&amp;nbsp; applications containing up to 128KB of code into an LPC target. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I did register. I am getting conflicting messages here, besides the one that the free version is limited.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Redoing the whole procedure again...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:53:10 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:53:10Z</dc:date>
    <item>
      <title>8K Limit and linker errors</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539197#M6394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cwpjr on Wed Jan 23 19:49:47 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;After object files were compiled&amp;nbsp; without error in V5 8k limit version the link phase complained of 2 major issues:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) ...axf section `.text' will not fit in region `MFlash32'. Is this saying the image is to large? The project is the simplest c main calling a larger .s file. Is the 8k limit for both c and asm?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2) The linker then indicates a group of undefined reference to say x, y and z seperately. Clicking on anyone&amp;nbsp; goes back to a source line where the hover over lists &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Multiple markers at this line&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- undefined reference to x&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- undefined reference to y&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- undefined reference to z&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;yet the the line is usually a branch to label with no linkage to the flagged x, y or z.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539197#M6394</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: 8K Limit and linker errors</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539198#M6395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gbm on Thu Jan 24 00:47:50 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Why don't you read the messages displayed during startup of LPCxpresso and register your software for free to remove the 8 K limit?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539198#M6395</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: 8K Limit and linker errors</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539199#M6396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by cwpjr on Thu Jan 24 14:20:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Launch CR V5,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Initial Msg Box:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;License type: UNACTIVATED (Activation not completed)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Debug limit: 8k &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Activation code: not available &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Welcome screen:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]LPCXpresso5 is fully activated[/B]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; Welcome to LPCXpresso 5. The software is now fully activated,&amp;nbsp; and can be used for production. LPCXpresso can be used to generate and download&amp;nbsp; applications containing up to 128KB of code into an LPC target. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I did register. I am getting conflicting messages here, besides the one that the free version is limited.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Redoing the whole procedure again...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/8K-Limit-and-linker-errors/m-p/539199#M6396</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:53:10Z</dc:date>
    </item>
  </channel>
</rss>