<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: SPI Interface and Debugging</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536088#M4903</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Oct 05 03:53:44 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]LPC-Link[/B]&amp;nbsp; does not support serial wire trace functionality of the Cortex-M3 processor within the LPC1343 thus SWO (also known as SWV) is not required for "normal debugging".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However if you ever intend to use your board with the Red Trace functionality of the full Red Suite with a RedProbe+ (rather than just using LPCXpresso IDE with LPC-Link), or equivalents from other companies, then be aware that this trace functionality would require SWO/SWV.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:09:34 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:09:34Z</dc:date>
    <item>
      <title>SPI Interface and Debugging</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536086#M4901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ALeicht on Tue Oct 05 02:19:33 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=4]Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a question about using the SPI Bus (on LPC1343) and the LPCxpresso debugging interface:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As I can see in the schematics the SPI Line "MOSI" is shared with the "SWO" Line used by the LPC-Link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to debug and use the SPI Bus at the same Time ? Or will the debugger disturb the SPI Communication ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Are there any layout recommendations I must take into account ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alex[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536086#M4901</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:09:33Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Interface and Debugging</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536087#M4902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Tue Oct 05 02:46:30 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso doesn't use SWO :)! So debugging is no problem. If you draw your own board, don't wire it to SWD-connector.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536087#M4902</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:09:33Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Interface and Debugging</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536088#M4903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Oct 05 03:53:44 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[B]LPC-Link[/B]&amp;nbsp; does not support serial wire trace functionality of the Cortex-M3 processor within the LPC1343 thus SWO (also known as SWV) is not required for "normal debugging".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However if you ever intend to use your board with the Red Trace functionality of the full Red Suite with a RedProbe+ (rather than just using LPCXpresso IDE with LPC-Link), or equivalents from other companies, then be aware that this trace functionality would require SWO/SWV.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Interface-and-Debugging/m-p/536088#M4903</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:09:34Z</dc:date>
    </item>
  </channel>
</rss>