<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Error 37 while browsing Registers tab</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535845#M4790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Sun May 15 09:35:31 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't see how the compiler optimisation level could have any affect like this. Can you zip up and post the .log file from the .metadata folder in your workspace?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, it would be interesting to know if you see the same issue using the current LPCXpresso IDE v8.1.4?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:25:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:25:54Z</dc:date>
    <item>
      <title>Error 37 while browsing Registers tab</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535844#M4789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robert hulsebos on Thu May 12 02:29:40 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We are using LPCXpresso v7.9.2 for building various LPC1769 projects. With one project we have hard fault situation that I am investigating. The fault occurs only when the compiler optimization setting is set at -Os (optimize for size), it does not occur when I set it at other levels. (for example -O3)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem I have is with the Registers tab of the Develop perspective: When using -O3 optimization, all works well and all registers on the Registers tab are displayed as expected. When I debug the same code, but this time compiled with -Os, then an &lt;/SPAN&gt;&lt;I&gt;'error 37: unknown peripheral name : faults&lt;/I&gt;&lt;SPAN&gt;' message is displayed while trying to browse the processor registers. The attachment contains all relevant screen copies... it is an annoying bug, as especially in the situation of a fault one would like to inspect the fault registers... &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535844#M4789</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error 37 while browsing Registers tab</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535845#M4790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Sun May 15 09:35:31 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't see how the compiler optimisation level could have any affect like this. Can you zip up and post the .log file from the .metadata folder in your workspace?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, it would be interesting to know if you see the same issue using the current LPCXpresso IDE v8.1.4?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535845#M4790</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: Error 37 while browsing Registers tab</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535846#M4791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:10:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Error-37-while-browsing-Registers-tab/m-p/535846#M4791</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:10:55Z</dc:date>
    </item>
  </channel>
</rss>