<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic c_type librarybeing compiled in in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535596#M4691</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andy on Thu Feb 03 23:21:55 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a project which compiles and runs using lpcxpresso under linux (version 3.8.2) which does not compile in the c_type library. so I can reasonably assume it is not needed,&amp;nbsp; but under windows (version 3.5.0 and 3.6.2)&amp;nbsp; it does using an additional 824bytes of flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;is this due to the different versions of gcc and can I add a another compiler option to fix this ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 03:00:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T03:00:57Z</dc:date>
    <item>
      <title>c_type librarybeing compiled in</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535596#M4691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andy on Thu Feb 03 23:21:55 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a project which compiles and runs using lpcxpresso under linux (version 3.8.2) which does not compile in the c_type library. so I can reasonably assume it is not needed,&amp;nbsp; but under windows (version 3.5.0 and 3.6.2)&amp;nbsp; it does using an additional 824bytes of flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;is this due to the different versions of gcc and can I add a another compiler option to fix this ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 03:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535596#M4691</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T03:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: c_type librarybeing compiled in</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535597#M4692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Feb 04 00:24:52 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The Linux version of LPCXpresso uses an updated version of Redlib compared to the Windows version, which provides some code and data size saving from a number of internal changes - including the ctype one that you note.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There is some more information on the new "Redlib_v2" at:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/redlib_v2_notes&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We are working at bringing the two versions into line in a forthcoming&amp;nbsp; new version of the tools. However I can't make any comment at present as&amp;nbsp; to when this will be released.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 03:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535597#M4692</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T03:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: c_type librarybeing compiled in</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535598#M4693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdseymour on Fri Feb 11 18:04:43 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm struggling with this same issue. Does anyone know of a workaround to keep the ctype module from being linked in?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 03:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/c-type-librarybeing-compiled-in/m-p/535598#M4693</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T03:00:58Z</dc:date>
    </item>
  </channel>
</rss>