<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Add more current with 2 pins in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535573#M4690</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Fri Jul 08 04:35:55 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Serge is right.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I mostly use th lpc1754 so almost have forgotten about my nice lpc1343 boards...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet specifies:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]High-current output driver (20 mA) on one pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So there is actually only 1 pin (PIO0_7) that is able to drive 20 mA. The other pins are limited to 4 mA (and no, it is still not a good idea to put 8 of these in parallel ;))&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:41:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:41:28Z</dc:date>
    <item>
      <title>Add more current with 2 pins</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535570#M4687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by volter on Thu Jul 07 13:14:07 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a Relay in my circuit and for get it work I need about 30mA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I know, all GPIO pins can generate 20mA so can I use 2 pins to control 1 part by simply connect them together :eek:?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535570#M4687</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:41:26Z</dc:date>
    </item>
    <item>
      <title>Re: Add more current with 2 pins</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535571#M4688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Thu Jul 07 13:24:53 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;that is a very bad idea.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Use a mosfet like a BS170 and a schottky diode .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you value the correct working of your microcontroller you will never drive a relay directly from the I/O pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535571#M4688</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Add more current with 2 pins</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535572#M4689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by serge on Thu Jul 07 23:36:10 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Isn't it so that for example the LPC1343 has only one (1) pin which can drive a led? Or did i misread the user manual?:confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And of course it is always better to use a fet or transistor to drive a relay.:p&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535572#M4689</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Add more current with 2 pins</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535573#M4690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Fri Jul 08 04:35:55 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Serge is right.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I mostly use th lpc1754 so almost have forgotten about my nice lpc1343 boards...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet specifies:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]High-current output driver (20 mA) on one pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So there is actually only 1 pin (PIO0_7) that is able to drive 20 mA. The other pins are limited to 4 mA (and no, it is still not a good idea to put 8 of these in parallel ;))&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Add-more-current-with-2-pins/m-p/535573#M4690</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:41:28Z</dc:date>
    </item>
  </channel>
</rss>