<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART and LPCXpresso in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534664#M4219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fpg on Wed May 11 08:27:20 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've got also a problem with LPCXpresso Baseboard UART, but with UART2 (the one which is handled through an i2c/spi to uart chip). As I looked at the project I should get messages from the board with HyperTerminal with the settings 115200 bps, 5 databits, no parity bit, 1 stop bit and no flow control. Yet I don't see anything.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't see, what I am missing...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:52:09 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:52:09Z</dc:date>
    <item>
      <title>UART and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534662#M4217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kubov on Fri Apr 22 03:52:55 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, this is my first post so firstly i want to introduce myself, my name is Jakub and I am from Poland, in advance i want to apologize for my English, sometimes it might by really painful to read my posts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, I am experiencing weird UART problem with LPCXpresso base board from embedded artists with LPC1343 micro-controller. I've compiled some example programs (uart, uart2 from embedded artists, and demo from embedded artists), each one is using an UART interface, but it doesn't work!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've done everything that manual said, installed FTDI drivers, setted up virtual COM port, but I cant even receive a single byte!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Steps I've made is: compile some program-&amp;gt;run putty with serial interface-&amp;gt;and the board just froze. I just want to add that the LEDS on board (near FTDI chip) are blinking during the transmission.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S I think that vendors gave to much abstraction level to device, can someone point me at some low level arm development papers (inb4 source code)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT0:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've checked it on Linux, the same thing, board just froze, and the LEDS are blinking as usual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT1:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;do you think, that this is the thing? &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.ftdichip.com/Support/Knowledgebase/index.html?windowsxpft232bmorft245bmdevic.htm&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EDIT2:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It was the issue with J54 jumper.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534662#M4217</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: UART and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534663#M4218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Fri Apr 22 11:34:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;kubov, Welcome to the forum.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The base board needs it's own power.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you have a separate USB cable or other external power attached to it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Larry&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:52:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534663#M4218</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:52:08Z</dc:date>
    </item>
    <item>
      <title>Re: UART and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534664#M4219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fpg on Wed May 11 08:27:20 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've got also a problem with LPCXpresso Baseboard UART, but with UART2 (the one which is handled through an i2c/spi to uart chip). As I looked at the project I should get messages from the board with HyperTerminal with the settings 115200 bps, 5 databits, no parity bit, 1 stop bit and no flow control. Yet I don't see anything.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't see, what I am missing...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534664#M4219</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:52:09Z</dc:date>
    </item>
    <item>
      <title>Re: UART and LPCXpresso</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534665#M4220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersrosvall on Thu May 12 00:39:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Check jumpers and check that you actually have 8 databits (not 5 as you wrote). Contact EA support for further assistance.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-and-LPCXpresso/m-p/534665#M4220</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:52:09Z</dc:date>
    </item>
  </channel>
</rss>