<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic msc_rom example bug update in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/msc-rom-example-bug-update/m-p/534476#M4119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ehughes on Tue Feb 08 18:42:25 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been trying to get to the bottom of why the msc_rom example doesn't work with windows 7.&amp;nbsp;&amp;nbsp; It was originally state on the forum hta tit might be because of the FAT 12 format.&amp;nbsp;&amp;nbsp; I don't bleieve this is true as the "bootloader" seems to enumerate/wok just fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a 1343 xpresso board where I wired a M25PE16 device into the PIport.&amp;nbsp; I have gotten this device to read/write properly.&amp;nbsp; My goal is to get a 2MB flash drive with the built in ROM code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; My hardware has a 1k resistor on the D+ line to +3.3v as required.&amp;nbsp; I am also first starting the program and then connectin the USB cable (per instructions if one does not use the soft connect feature).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I notice that when I plug the device into a USB port,&amp;nbsp; the program will jump to the "HardFault"&amp;nbsp; irq handler continuously.&amp;nbsp;&amp;nbsp; This is true under Wwindows XP and Windows 7.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure what this means but I am going to look down that trail for awhile....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:59:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:59:50Z</dc:date>
    <item>
      <title>msc_rom example bug update</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/msc-rom-example-bug-update/m-p/534476#M4119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ehughes on Tue Feb 08 18:42:25 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have been trying to get to the bottom of why the msc_rom example doesn't work with windows 7.&amp;nbsp;&amp;nbsp; It was originally state on the forum hta tit might be because of the FAT 12 format.&amp;nbsp;&amp;nbsp; I don't bleieve this is true as the "bootloader" seems to enumerate/wok just fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a 1343 xpresso board where I wired a M25PE16 device into the PIport.&amp;nbsp; I have gotten this device to read/write properly.&amp;nbsp; My goal is to get a 2MB flash drive with the built in ROM code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; My hardware has a 1k resistor on the D+ line to +3.3v as required.&amp;nbsp; I am also first starting the program and then connectin the USB cable (per instructions if one does not use the soft connect feature).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I notice that when I plug the device into a USB port,&amp;nbsp; the program will jump to the "HardFault"&amp;nbsp; irq handler continuously.&amp;nbsp;&amp;nbsp; This is true under Wwindows XP and Windows 7.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure what this means but I am going to look down that trail for awhile....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/msc-rom-example-bug-update/m-p/534476#M4119</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:59:50Z</dc:date>
    </item>
  </channel>
</rss>