<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピック8 bit aligned GPIO port?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/8-bit-aligned-GPIO-port/m-p/533413#M3607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jcottier on Fri Feb 10 07:34:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, I am using an LPC122x device, and I would like to split the 32 bit GPIO port into 1 or more 8 bit aligned GPIO ports (EG an LCD controller port). For example so I can directly output D0-D7 data to GPIO bits 8-15 without any bit shifting. Is that possible on this device?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:59:48 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:59:48Z</dc:date>
    <item>
      <title>8 bit aligned GPIO port?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/8-bit-aligned-GPIO-port/m-p/533413#M3607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jcottier on Fri Feb 10 07:34:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, I am using an LPC122x device, and I would like to split the 32 bit GPIO port into 1 or more 8 bit aligned GPIO ports (EG an LCD controller port). For example so I can directly output D0-D7 data to GPIO bits 8-15 without any bit shifting. Is that possible on this device?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/8-bit-aligned-GPIO-port/m-p/533413#M3607</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:59:48Z</dc:date>
    </item>
  </channel>
</rss>