<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 53: License does not permit flash operations from the command line? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533140#M3453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mosesmck on Fri Oct 08 11:30:33 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just got an LPCXpresso with the LPC1114 chip on it, and I'm using LPCXpresso for Linux Beta 2 on Ubuntu 10.04.&amp;nbsp; I compiled the "Blinky" example in debug mode and tried to write it to the chip using the "Program Flash" button, and it gives me the following error in a message box:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"53: License does not permit flash operations from the command line"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I got the license for the free version of LPCXpresso, and the welcome page tells me:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Welcome to LPCXpresso.&amp;nbsp; The software is now fully activated, and can be used for production.&amp;nbsp; LPCXpresso can be used to generate and download applications containing up to 128K of code into an LPC target."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was able to run the program in Debug mode and that wrote the program to the chip, but I really would like to be able to just program the flash.&amp;nbsp; Does anyone know what might be the problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Moses&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:08:16 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:08:16Z</dc:date>
    <item>
      <title>53: License does not permit flash operations from the command line?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533140#M3453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mosesmck on Fri Oct 08 11:30:33 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just got an LPCXpresso with the LPC1114 chip on it, and I'm using LPCXpresso for Linux Beta 2 on Ubuntu 10.04.&amp;nbsp; I compiled the "Blinky" example in debug mode and tried to write it to the chip using the "Program Flash" button, and it gives me the following error in a message box:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"53: License does not permit flash operations from the command line"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I got the license for the free version of LPCXpresso, and the welcome page tells me:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Welcome to LPCXpresso.&amp;nbsp; The software is now fully activated, and can be used for production.&amp;nbsp; LPCXpresso can be used to generate and download applications containing up to 128K of code into an LPC target."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I was able to run the program in Debug mode and that wrote the program to the chip, but I really would like to be able to just program the flash.&amp;nbsp; Does anyone know what might be the problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Moses&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533140#M3453</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:16Z</dc:date>
    </item>
    <item>
      <title>Re: 53: License does not permit flash operations from the command line?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533141#M3454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Sat Oct 09 01:58:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First of all, are you running, the 32-bit or 64-bit version of Ubuntu 10.04?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Next, can you try re-activating. That is, get the serial number and (if it is different to the one you already have), get a new activation code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If that doesn't solve the problem, can you run "crt_emu_cm3_nxp -info-license" from a shell, and then zip and post the whole directory "/usr/share/LPCXpresso".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533141#M3454</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: 53: License does not permit flash operations from the command line?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533142#M3455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mosesmck on Mon Oct 11 16:34:09 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm running 32-bit version of Ubuntu.&amp;nbsp; I just had to reactivate because lightning took out the onboard NIC on this computer last night and I put in a new card.&amp;nbsp; The IDE came up and said it was not activated, so I re-activated and now I can directly program the flash.&amp;nbsp; I guess it was a problem with the first activation!&amp;nbsp; Maybe the licensing stuff likes 3Com cards better than onboard NICs???&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Moses&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533142#M3455</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: 53: License does not permit flash operations from the command line?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533143#M3456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 00:41:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i am using 64 bit windows 7. I was able to run the program in the Debug mode. But it is not possible to use the "Program Flash" option.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am getting an error like this:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"53: License does not permit flash operations from the command line"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried reactivation also. But still i am getting the same problem.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/53-License-does-not-permit-flash-operations-from-the-command/m-p/533143#M3456</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:08:18Z</dc:date>
    </item>
  </channel>
</rss>