<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC Link2 COM port</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/1444850#M33352</link>
    <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;VCOM port mostly will solve the issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://mycfavisit.site/" target="_self"&gt;&lt;SPAN&gt;https://mycfavisit.site&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Apr 2022 11:16:04 GMT</pubDate>
    <dc:creator>prakashxd</dc:creator>
    <dc:date>2022-04-18T11:16:04Z</dc:date>
    <item>
      <title>LPC Link2 COM port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/542222#M7752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dalzan on Tue May 17 15:45:50 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am a beginner with LPC/ARM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I connect LPC Link2 via USB to my computer and launch Debug there appear 2 "HID Standard Devices" / "CMSIS-DAP" and "LPC-SIO Port", and also "Ports (COM and LPT)" / "LPC-LinkII UCom Port (COM3)". Maybe also some others I haven't noticed..&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do I understand right the HID interface is used for JTAG/SWD debugger and the port COM3 is free to use ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I see on the schematic diagram of Link2 that "Serial Expansion Interface" connector J3 contains pins UART2_RXD + UART2_TXD;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;when I open this COM3 with TeraTerm or other UART terminal and enter some text, will it be transmitted to this UART2_TXD ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I know I could test it myself, problem is with the 50mils fine pitch headers, not so easy to connect anything here quickly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My plan is to interconnect Link2 (UART2 pins mentioned above) with NGX LPC-4330-Xplorer / connector J8 / pins 9,10 == U0_TXD+U0_RXD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then I could test application with UART output without a need for additional TTL-&amp;gt;UART-&amp;gt;USB converter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any comments appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/542222#M7752</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:51:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link2 COM port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/542223#M7753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default firmware for the standalone LPC-Link2 uses the same port pins as the on-board version, which are P2_0 and P2_1. When LPC-Link2 was initially designed there was a long term goal to support parallel trace, which was never implement as HS USB bandwidth and available SRAM was seen as too limiting; ports P2_0 and P2_1 were used as trace port connections to the target via a buffer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to get a unidirectional VCOM port (from a target to the host PC via LPC-Link2) by connecting to pin 16 of the SWD/JTAG/ETM connector J8 at pin 16.&amp;nbsp;Due to the buffer between the LPC4370 on LPC-Link2 (originally intended for trace data), it is not possible to get data in the other direction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 19:06:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/542223#M7753</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2019-12-20T19:06:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link2 COM port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/1249138#M33289</link>
      <description>&lt;P&gt;&lt;SPAN&gt;HS USB bandwidth and available SRAM was seen as too limiting; ports P2_0 and P2_1 were used as trace &lt;A href="https://testmyspeed.onl/" target="_self"&gt;testmyspeed.onl&lt;/A&gt; port connections to the target via a &amp;nbsp;buffer.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 20 Mar 2021 10:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/1249138#M33289</guid>
      <dc:creator>Kasey00</dc:creator>
      <dc:date>2021-03-20T10:57:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link2 COM port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/1444850#M33352</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;VCOM port mostly will solve the issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://mycfavisit.site/" target="_self"&gt;&lt;SPAN&gt;https://mycfavisit.site&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 11:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link2-COM-port/m-p/1444850#M33352</guid>
      <dc:creator>prakashxd</dc:creator>
      <dc:date>2022-04-18T11:16:04Z</dc:date>
    </item>
  </channel>
</rss>