<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No connection to emulator device? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/No-connection-to-emulator-device/m-p/777735#M33263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the NHS 3152 on the Eval-board "NHS3152THADADK", which has 13 switches. I changed the blinky demo software to get an output at GPIO 5 and 7. The other Pins I wanted to use as Inputs, to see whether I can detect my output signal on an Input pin, because of the internal connection caused by the switches.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After flashing my program I am not able anymore to connect to the microcontroller. I attached the code and the error message.&lt;/P&gt;&lt;P&gt;Somehow I think it was a bad idea to change the programming pins 10 and 11 to Input and that's why I can't connect to the core anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 10:05:00 GMT</pubDate>
    <dc:creator>raphaelprechtel</dc:creator>
    <dc:date>2017-12-11T10:05:00Z</dc:date>
    <item>
      <title>No connection to emulator device?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/No-connection-to-emulator-device/m-p/777735#M33263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the NHS 3152 on the Eval-board "NHS3152THADADK", which has 13 switches. I changed the blinky demo software to get an output at GPIO 5 and 7. The other Pins I wanted to use as Inputs, to see whether I can detect my output signal on an Input pin, because of the internal connection caused by the switches.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After flashing my program I am not able anymore to connect to the microcontroller. I attached the code and the error message.&lt;/P&gt;&lt;P&gt;Somehow I think it was a bad idea to change the programming pins 10 and 11 to Input and that's why I can't connect to the core anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 10:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/No-connection-to-emulator-device/m-p/777735#M33263</guid>
      <dc:creator>raphaelprechtel</dc:creator>
      <dc:date>2017-12-11T10:05:00Z</dc:date>
    </item>
  </channel>
</rss>