<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I2C is not working in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/I2C-is-not-working/m-p/738732#M33188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the NHS3152 and want to use the I²C bus. I have tested the example of NXP but it doesn't work. Also I tried my own programm based on the example, which isn't working, too.&lt;/P&gt;&lt;P&gt;Is the programm tested for this chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not even getting a clock signal at the SCL pin. But perhaps I am doing something completely wrong.&lt;/P&gt;&lt;P&gt;Here is my main:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "board.h"&lt;BR /&gt;#include "NHS+MAX.h"&lt;BR /&gt;#define I2C_MASTER&lt;BR /&gt;#ifdef I2C_MASTER&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #include "master.h"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_SYSTEMCLOCK == NSS_SFRO_FREQUENCY) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Flash_SetHighPowerMode(true);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Clock_System_SetClockFreq(I2C_SYSTEMCLOCK);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#ifdef I2C_MASTER&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Master_Init_NHS();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t MAX_ID;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (true) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;MasterRead_MAX(0xFF,0x57, (uint8_t*) &amp;amp;MAX_ID, sizeof(MAX_ID));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Clock_System_BusyWait_ms(I2C_MASTER_COMM_INTERVAL);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("%i \n", MAX_ID);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;#endif&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to read the id of a MAX30101 Sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone could help me, that would be great!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Dec 2017 14:44:48 GMT</pubDate>
    <dc:creator>raphaelprechtel</dc:creator>
    <dc:date>2017-12-20T14:44:48Z</dc:date>
    <item>
      <title>I2C is not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/I2C-is-not-working/m-p/738732#M33188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the NHS3152 and want to use the I²C bus. I have tested the example of NXP but it doesn't work. Also I tried my own programm based on the example, which isn't working, too.&lt;/P&gt;&lt;P&gt;Is the programm tested for this chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not even getting a clock signal at the SCL pin. But perhaps I am doing something completely wrong.&lt;/P&gt;&lt;P&gt;Here is my main:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "board.h"&lt;BR /&gt;#include "NHS+MAX.h"&lt;BR /&gt;#define I2C_MASTER&lt;BR /&gt;#ifdef I2C_MASTER&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #include "master.h"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_SYSTEMCLOCK == NSS_SFRO_FREQUENCY) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Flash_SetHighPowerMode(true);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Clock_System_SetClockFreq(I2C_SYSTEMCLOCK);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#ifdef I2C_MASTER&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Master_Init_NHS();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t MAX_ID;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (true) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;MasterRead_MAX(0xFF,0x57, (uint8_t*) &amp;amp;MAX_ID, sizeof(MAX_ID));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_Clock_System_BusyWait_ms(I2C_MASTER_COMM_INTERVAL);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("%i \n", MAX_ID);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;#endif&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to read the id of a MAX30101 Sensor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If someone could help me, that would be great!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2017 14:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/I2C-is-not-working/m-p/738732#M33188</guid>
      <dc:creator>raphaelprechtel</dc:creator>
      <dc:date>2017-12-20T14:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: I2C is not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/I2C-is-not-working/m-p/738733#M33189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raphael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you resolved the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also met some similar issue when using I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you be kindly to share your experience if you solved the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Arna&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 06:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/I2C-is-not-working/m-p/738733#M33189</guid>
      <dc:creator>aresmarser</dc:creator>
      <dc:date>2018-03-16T06:02:11Z</dc:date>
    </item>
  </channel>
</rss>