<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: In which file are the Build configurations?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/In-which-file-are-the-Build-configurations/m-p/687097#M32987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So you deleted a project, then expected to still be able to use it? Not something we would generally recommend - certainly without making a backup first (for example by using the Quickstart -&amp;gt; Export to zip option) !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also not sure that I follow why you think this is a good thing to describe to a new employee.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That aside, I have just tried the process that you describe, and my project imported back into the workspace appears to function correctly. The only thing that I can think of is that you managed to delete or modify 1 or more of the files from within the project itself somehow (in particular the .cproject and/or .project), rather than just deleting the metadata that describes the project's&amp;nbsp;existence&amp;nbsp;in the workspace&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry to say that you be&amp;nbsp;better off creating a new project, then copying the files from your original project into it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jul 2017 08:31:22 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-07-07T08:31:22Z</dc:date>
    <item>
      <title>In which file are the Build configurations?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/In-which-file-are-the-Build-configurations/m-p/687096#M32986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPCXpresso V8.2.0 for LPC812. My project was working fine. I wanted to write a document on how to setup the software for a new employee, so I deleted the project by right-clicking and "Delete". &lt;BR /&gt;After I clicked on File-Import. Under "General", I chose "Existing Projects into Workspace" and selected the folder where my project is.&lt;BR /&gt;When I go to my build configurations, I only see "Default". Before, I had "Debug" and "Release".&lt;BR /&gt;Also, I cannot compile anymore, I have the error "Error: Program "make" not found in PATH".&lt;/P&gt;&lt;P&gt;I really need this to work as soon as possible!&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 18:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/In-which-file-are-the-Build-configurations/m-p/687096#M32986</guid>
      <dc:creator>martinpare</dc:creator>
      <dc:date>2017-07-06T18:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: In which file are the Build configurations?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/In-which-file-are-the-Build-configurations/m-p/687097#M32987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So you deleted a project, then expected to still be able to use it? Not something we would generally recommend - certainly without making a backup first (for example by using the Quickstart -&amp;gt; Export to zip option) !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also not sure that I follow why you think this is a good thing to describe to a new employee.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That aside, I have just tried the process that you describe, and my project imported back into the workspace appears to function correctly. The only thing that I can think of is that you managed to delete or modify 1 or more of the files from within the project itself somehow (in particular the .cproject and/or .project), rather than just deleting the metadata that describes the project's&amp;nbsp;existence&amp;nbsp;in the workspace&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry to say that you be&amp;nbsp;better off creating a new project, then copying the files from your original project into it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 08:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/In-which-file-are-the-Build-configurations/m-p/687097#M32987</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-07-07T08:31:22Z</dc:date>
    </item>
  </channel>
</rss>