<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPCXpresso MCUXpresso - CDT 9.2</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680309#M32955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, If MCUXpresso will be updated then I will move to soon. The reason I didn't do it is my full license on LPCXpresso. Is it possible to use the full license with MCUXpresso?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jun 2017 07:03:47 GMT</pubDate>
    <dc:creator>abderrezak</dc:creator>
    <dc:date>2017-06-09T07:03:47Z</dc:date>
    <item>
      <title>LPCXpresso MCUXpresso - CDT 9.2</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680307#M32953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I develop many projects around NXP uC and I use for this LPCXpresso (soon I'll move to MCUXpresso).&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have reported a bug/feature to eclipse.&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://bugs.eclipse.org/bugs/show_bug.cgi?id=517954" title="https://bugs.eclipse.org/bugs/show_bug.cgi?id=517954"&gt;Bug 517954 – auto-complete of parameters generates ClassCastException on function pointers&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://bugs.eclipse.org/bugs/show_bug.cgi?id=517978" title="https://bugs.eclipse.org/bugs/show_bug.cgi?id=517978"&gt;Bug 517978 – Provide completion proposal based on function pointer's type&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The requsted feature will be implemented in the eclipse CDT 9.2.&lt;/P&gt;&lt;P&gt;I wish to know if LPCXpresso or MCUXpresso will use the new version of eclipse CDT 9.2. If yes it's well, otherwise can I by my own install the newer CDT in the NXP-IDEs installation to have access to that feature.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 08:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680307#M32953</guid>
      <dc:creator>abderrezak</dc:creator>
      <dc:date>2017-06-08T08:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso MCUXpresso - CDT 9.2</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680308#M32954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although it would theoretically possible for a user to update&amp;nbsp;the version of CDT used in our IDEs, this is not something we would recommend or support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will be updating the CDT version used by MCUXpresso IDE from the current CDT 9.1 in a future release, though we can't currently give details of&amp;nbsp;the date of the change or&amp;nbsp;the exact version we'll be moving to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 20:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680308#M32954</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-06-08T20:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso MCUXpresso - CDT 9.2</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680309#M32955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, If MCUXpresso will be updated then I will move to soon. The reason I didn't do it is my full license on LPCXpresso. Is it possible to use the full license with MCUXpresso?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 07:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680309#M32955</guid>
      <dc:creator>abderrezak</dc:creator>
      <dc:date>2017-06-09T07:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso MCUXpresso - CDT 9.2</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680310#M32956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An LPCXpresso IDE Pro Edition license will also activate MCUXpresso IDE in Pro Edition mode. You can have the two installed in parallel on the same machine too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details of the differences between the two IDEs, please refer to the MCUXpresso IDE Installation Guide, downloadable from -&amp;nbsp;&lt;A class="link-titled" href="http://www.nxp.com/mcuxpresso/ide/documentation" title="http://www.nxp.com/mcuxpresso/ide/documentation"&gt;MCUXpresso IDE|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 07:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-MCUXpresso-CDT-9-2/m-p/680310#M32956</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-06-09T07:32:59Z</dc:date>
    </item>
  </channel>
</rss>