<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Systick register, not showing in debug!!! in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Systick-register-not-showing-in-debug/m-p/673719#M32908</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello to all,&lt;/P&gt;&lt;P&gt;From the piece of code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Enable SysTick Timer */&lt;BR /&gt; SysTick_Config(SystemCoreClock / TICKRATE_HZ);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, while debugging, can't see the register responsible for that. Do we need to enable some kind of register by coding in our main function???&lt;/P&gt;&lt;P&gt;#Systick-Register-enable&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 06:50:18 GMT</pubDate>
    <dc:creator>himanshudoshi</dc:creator>
    <dc:date>2017-07-19T06:50:18Z</dc:date>
    <item>
      <title>Systick register, not showing in debug!!!</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Systick-register-not-showing-in-debug/m-p/673719#M32908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello to all,&lt;/P&gt;&lt;P&gt;From the piece of code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Enable SysTick Timer */&lt;BR /&gt; SysTick_Config(SystemCoreClock / TICKRATE_HZ);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, while debugging, can't see the register responsible for that. Do we need to enable some kind of register by coding in our main function???&lt;/P&gt;&lt;P&gt;#Systick-Register-enable&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 06:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Systick-register-not-showing-in-debug/m-p/673719#M32908</guid>
      <dc:creator>himanshudoshi</dc:creator>
      <dc:date>2017-07-19T06:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: Systick register, not showing in debug!!!</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Systick-register-not-showing-in-debug/m-p/673720#M32909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You don't say which part you are using, but for most MCUs, the Systick registers are provided within the NVIC peripheral (as that is where the live within the memory map).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 10:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Systick-register-not-showing-in-debug/m-p/673720#M32909</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-07-19T10:20:28Z</dc:date>
    </item>
  </channel>
</rss>