<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC4330FBD144, Problems booting from reset and cold</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330FBD144-Problems-booting-from-reset-and-cold/m-p/669632#M32872</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When testing another board we could not find these problems so i've come to the cunclusion that something was wrong with the other board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this thread could be closed as problem is resolved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Jul 2017 19:12:20 GMT</pubDate>
    <dc:creator>hansod</dc:creator>
    <dc:date>2017-07-16T19:12:20Z</dc:date>
    <item>
      <title>LPC4330FBD144, Problems booting from reset and cold</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330FBD144-Problems-booting-from-reset-and-cold/m-p/669631#M32871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've designed a custom board using an LCP4330 and trying to some leds to turn on as a first step. All was fine downloading the image with the debugger LPC-LINK2 and the program started ok and the leds lit up. Then i wanted to try resetting the board and no leds were turning on. If i powercycle the board same thing, no leds turning on so i assume the application is not running or something else is wrong.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OTP_BOOT_SRC is not programmed and P2_9,P2_8,P1_2 is pulled down, P1_1 is pulled high so we should boot from SPIFI, P2_7 is pulled high so i should not enter ISP.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using LPCXpresso v8.2.2_650 and have based my code from the existing LPC4330 examples. I have only downloaded the application with the debugger. The SPIFI chip is S25FL127SABMFI101.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have put in a few days debugging the problem but now i need to ask for help. What can cause the LPC4330 not to boot and reset&amp;nbsp;from SPIFI if all bootpins etc is correct? Do i need to program or build the application in a certain way? Is my application not correct? I modified the ResetISR so the first thing i do is setting the leds and then go into a while loop with __asm("nop"). This works when doing a debug session but not with doing reset or cold start.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have traced the pins on the SPIFI chip with a Saleae Logic Analyzer&amp;nbsp; when doing a reset and some activity is there, but if its good i have no clue about. I'm attaching the trace, project etc so maybe someone can help me figure this out.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards / Hans&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338173"&gt;Project.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338173"&gt;Trace_logic_reset.logicdata.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2017 21:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330FBD144-Problems-booting-from-reset-and-cold/m-p/669631#M32871</guid>
      <dc:creator>hansod</dc:creator>
      <dc:date>2017-07-13T21:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330FBD144, Problems booting from reset and cold</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330FBD144-Problems-booting-from-reset-and-cold/m-p/669632#M32872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When testing another board we could not find these problems so i've come to the cunclusion that something was wrong with the other board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So this thread could be closed as problem is resolved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Jul 2017 19:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330FBD144-Problems-booting-from-reset-and-cold/m-p/669632#M32872</guid>
      <dc:creator>hansod</dc:creator>
      <dc:date>2017-07-16T19:12:20Z</dc:date>
    </item>
  </channel>
</rss>