<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCxpresso segmentation fault on startup on Ubuntu LTS in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667694#M32868</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure you have read the Linux installation notes in the LPCXpresso IDE Installation Guide - or else at&amp;nbsp;&lt;A href="https://community.nxp.com/message/630634"&gt;https://community.nxp.com/message/630634&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That aside, this version of Ubuntu post-dates the last LPCXpresso IDE update. You might want to consider using the replacement MCUXpresso IDE instead if this is for a new project. The Ubuntu installer for this has been reworked completely compared to the old LPCXpresso IDE installer, and it is now also a 64bit application rather than 32bit - which makes installing much easier on 64bit systems. For more details visit &lt;A href="http://www.nxp.com/mcuxpresso/ide"&gt;http://www.nxp.com/mcuxpresso/ide&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Jun 2017 10:23:54 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-06-21T10:23:54Z</dc:date>
    <item>
      <title>LPCxpresso segmentation fault on startup on Ubuntu LTS</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667693#M32867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE&gt;# lpcxpresso 
Segmentation fault

# uname -a 
Linux javox-linux-pc 4.4.0-81-generic #104-Ubuntu SMP Wed Jun 14 08:17:06 UTC 2017 x86_64 x86_64 x86_64 GNU/Linux

# cat /etc/issue
Ubuntu 16.04.2 LTS \n \l

# strace lpcxpresso[...SNIP...]clone(child_stack=0xd2fe0424, flags=CLONE_VM|CLONE_FS|CLONE_FILES|CLONE_SIGHAND|CLONE_THREAD|CLONE_SYSVSEM|CLONE_SETTLS|CLONE_PARENT_SETTID|CLONE_CHILD_CLEARTID, parent_tidptr=0xd2fe0ba8, tls={entry_number:12, base_addr:0xd2fe0b40, limit:1048575, seg_32bit:1, contents:0, read_exec_only:0, limit_in_pages:1, seg_not_present:0, useable:1}, child_tidptr=0xd2fe0ba8) = 6939
futex(0x93f7a44, FUTEX_WAIT_PRIVATE, 1, NULL) = 0
futex(0x93f7a28, FUTEX_WAKE_PRIVATE, 1) = 0
futex(0x944e044, FUTEX_WAKE_OP_PRIVATE, 1, 1, 0x944e040, {FUTEX_OP_SET, 0, FUTEX_OP_CMP_GT, 1}) = 1
futex(0x944e028, FUTEX_WAKE_PRIVATE, 1) = 1
futex(0x944e044, FUTEX_WAKE_OP_PRIVATE, 1, 1, 0x944e040, {FUTEX_OP_SET, 0, FUTEX_OP_CMP_GT, 1}) = 1
futex(0x944e028, FUTEX_WAKE_PRIVATE, 1) = 1
--- SIGSEGV {si_signo=SIGSEGV, si_code=SEGV_MAPERR, si_addr=0xffff0728} ---
rt_sigprocmask(SIG_SETMASK, ~[RTMIN RT_1], ~[KILL STOP RTMIN RT_1], 8) = 0
--- SIGSEGV {si_signo=SIGSEGV, si_code=SEGV_MAPERR, si_addr=0xffff0fe0} ---
+++ killed by SIGSEGV +++
Segmentation fault

# tail /var/log/apt/history.log
[...SNIP...]
Start-Date: 2017-06-20 10:26:09
Install: linux-image-4.4.0-81-generic:amd64 (4.4.0-81.104, automatic), linux-headers-4.4.0-81:amd64 (4.4.0-81.104, automatic), linux-image-extra-4.4.0-81-generic:amd64 (4.4.0-81.104, automatic), linux-headers-4.4.0-81-generic:amd64 (4.4.0-81.104, automatic)
Upgrade: linux-headers-generic:amd64 (4.4.0.79.85, 4.4.0.81.87), libc6-dev-x32:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), linux-libc-dev:amd64 (4.4.0-79.100, 4.4.0-81.104), libc6-dev-i386:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc6-dbg:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc6-dev:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), linux-image-generic:amd64 (4.4.0.79.85, 4.4.0.81.87), libc6:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc6:i386 (2.23-0ubuntu7, 2.23-0ubuntu9), locales:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc-bin:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc6-x32:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc6-i386:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), libc-dev-bin:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), multiarch-support:amd64 (2.23-0ubuntu7, 2.23-0ubuntu9), linux-generic:amd64 (4.4.0.79.85, 4.4.0.81.87)
End-Date: 2017-06-20 10:27:30




Any ideas? Thanks!&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 14:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667693#M32867</guid>
      <dc:creator>berndgeiser</dc:creator>
      <dc:date>2017-06-20T14:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso segmentation fault on startup on Ubuntu LTS</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667694#M32868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure you have read the Linux installation notes in the LPCXpresso IDE Installation Guide - or else at&amp;nbsp;&lt;A href="https://community.nxp.com/message/630634"&gt;https://community.nxp.com/message/630634&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That aside, this version of Ubuntu post-dates the last LPCXpresso IDE update. You might want to consider using the replacement MCUXpresso IDE instead if this is for a new project. The Ubuntu installer for this has been reworked completely compared to the old LPCXpresso IDE installer, and it is now also a 64bit application rather than 32bit - which makes installing much easier on 64bit systems. For more details visit &lt;A href="http://www.nxp.com/mcuxpresso/ide"&gt;http://www.nxp.com/mcuxpresso/ide&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 10:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667694#M32868</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-06-21T10:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso segmentation fault on startup on Ubuntu LTS</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667695#M32869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;mcuxpresso is the way to go. thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jun 2017 10:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667695#M32869</guid>
      <dc:creator>berndgeiser</dc:creator>
      <dc:date>2017-06-21T10:39:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso segmentation fault on startup on Ubuntu LTS</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667696#M32870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;using command bellow may be help you:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #111111; background-color: #eff0f1;"&gt;export JAVA_TOOL_OPTIONS=-Xss1280k&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 11:05:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-segmentation-fault-on-startup-on-Ubuntu-LTS/m-p/667696#M32870</guid>
      <dc:creator>quanghm</dc:creator>
      <dc:date>2017-06-27T11:05:42Z</dc:date>
    </item>
  </channel>
</rss>