<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Unable to connect to core</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662468#M32797</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You have probably got your chip into a strange state. This FAQ describes how to regain access:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389112"&gt;https://community.nxp.com/thread/389112&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Apr 2017 16:08:47 GMT</pubDate>
    <dc:creator>thefallguy</dc:creator>
    <dc:date>2017-04-10T16:08:47Z</dc:date>
    <item>
      <title>Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662467#M32796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPC-Link2 debugger with LPCXpresso v8.2.2 and have started seeing the following error while debugging:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nc: connecting to core 0 with handle 0x1 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x1 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x1 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: probe unbooted? no core 0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know what could be the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Prachi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 02:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662467#M32796</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-04-10T02:47:26Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662468#M32797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You have probably got your chip into a strange state. This FAQ describes how to regain access:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389112"&gt;https://community.nxp.com/thread/389112&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 16:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662468#M32797</guid>
      <dc:creator>thefallguy</dc:creator>
      <dc:date>2017-04-10T16:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662469#M32798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to the FAQ recommended by the Fall Guy, check to see if a rogue redlinkserv process exists. It can prevent access to the target. Once you see the reported error, check the process list. If you see a redlinkserv process but have no other debug connections active, kill the process and retry.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 18:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662469#M32798</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-04-10T18:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662470#M32799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. Using the Vector catch and the Reset handling options and by killling the redlinkserv process, I am able to connect back to the target sometimes. However, it is inconsistent and sometimes does not recover when these options are tried.&lt;/P&gt;&lt;P&gt;What can be tried further?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Prachi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2017 11:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662470#M32799</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-04-28T11:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662471#M32800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is your application actually doing anything in your system setup that could be putting your MCU into a "strange state" - as described at the top of the&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389112"&gt;https://community.nxp.com/thread/389112&lt;/A&gt;&amp;nbsp;FAQ ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What MCU and board are you using? I would certain suggest checking your debug and reset connections :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="https://community.nxp.com/thread/388998"&gt;Design Considerations for Debug&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you post debug logs for both working and non-working connections?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389146"&gt;The Debug Log&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 May 2017 08:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662471#M32800</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-05-02T08:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to connect to core</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662472#M32801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your help. The issue doesn't seem to occur much when the Enable Code Read Protection and the Link Application to RAM options are disabled.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2017 04:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Unable-to-connect-to-core/m-p/662472#M32801</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-05-18T04:06:28Z</dc:date>
    </item>
  </channel>
</rss>