<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックARM7 flash programming and debugging</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/ARM7-flash-programming-and-debugging/m-p/651077#M32715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to program an LPC2214 (ARM7tdmi)&amp;nbsp; from LPCXpresso V8.2.2, I was under the impression from your website that the CMSIS-DAP probe on the OM13085 board could be used for this as this is a replacement for the LPCXpresso V1 boards which are ARM7/9 compatible.We have purchased 2 boards, but LPCXpresso says that the "Debug probe not supported with this target" "Reason:LinkServer does not support NXP LPC2214/01 (arm7tdmi)"&lt;/P&gt;&lt;P&gt;How can I program an Arm7 device from LPCXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 12:07:37 GMT</pubDate>
    <dc:creator>andrewbromilow</dc:creator>
    <dc:date>2017-01-27T12:07:37Z</dc:date>
    <item>
      <title>ARM7 flash programming and debugging</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ARM7-flash-programming-and-debugging/m-p/651077#M32715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to program an LPC2214 (ARM7tdmi)&amp;nbsp; from LPCXpresso V8.2.2, I was under the impression from your website that the CMSIS-DAP probe on the OM13085 board could be used for this as this is a replacement for the LPCXpresso V1 boards which are ARM7/9 compatible.We have purchased 2 boards, but LPCXpresso says that the "Debug probe not supported with this target" "Reason:LinkServer does not support NXP LPC2214/01 (arm7tdmi)"&lt;/P&gt;&lt;P&gt;How can I program an Arm7 device from LPCXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 12:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ARM7-flash-programming-and-debugging/m-p/651077#M32715</guid>
      <dc:creator>andrewbromilow</dc:creator>
      <dc:date>2017-01-27T12:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: ARM7 flash programming and debugging</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ARM7-flash-programming-and-debugging/m-p/651078#M32716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately&amp;nbsp;LPCXpresso IDE only supports debugging ARM7 based MCUs using LPC-Link1 or Red Probe+&lt;BR /&gt;debug probes. It is not possible to use a CMSIS-DAP probe for ARM7 based MCU debugging. For more information, please see&amp;nbsp;the FAQ at - &lt;A _jive_internal="true" href="https://community.nxp.com/message/630901"&gt;https://community.nxp.com/message/630901&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 19:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ARM7-flash-programming-and-debugging/m-p/651078#M32716</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-01-27T19:35:12Z</dc:date>
    </item>
  </channel>
</rss>