<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPCXpresso Using ISP Uart Flash Program</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Using-ISP-Uart-Flash-Program/m-p/645830#M32662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am just starting using LPCXpresso IDE under Ubuntu 16.04LTS. I wonder if there is any way to program OnChip flash memory using ISP Uart BootLoader mode of the device. I am able to communicate with the chip using lpctools but I wonder if there is some way to integrate the flash programming phase inside the LPCXpresso IDE. I have a custom board and I have no jtag connection available. The only way to program the flash memory is using a Uart cable to download image to the device (using an USB -&amp;gt; Uart adapter that is working with lpctools).&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marco Bisio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Dec 2016 02:07:50 GMT</pubDate>
    <dc:creator>mrcbis</dc:creator>
    <dc:date>2016-12-28T02:07:50Z</dc:date>
    <item>
      <title>LPCXpresso Using ISP Uart Flash Program</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Using-ISP-Uart-Flash-Program/m-p/645830#M32662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am just starting using LPCXpresso IDE under Ubuntu 16.04LTS. I wonder if there is any way to program OnChip flash memory using ISP Uart BootLoader mode of the device. I am able to communicate with the chip using lpctools but I wonder if there is some way to integrate the flash programming phase inside the LPCXpresso IDE. I have a custom board and I have no jtag connection available. The only way to program the flash memory is using a Uart cable to download image to the device (using an USB -&amp;gt; Uart adapter that is working with lpctools).&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marco Bisio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 02:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Using-ISP-Uart-Flash-Program/m-p/645830#M32662</guid>
      <dc:creator>mrcbis</dc:creator>
      <dc:date>2016-12-28T02:07:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso Using ISP Uart Flash Program</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Using-ISP-Uart-Flash-Program/m-p/645831#M32663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nothing in the ide, but try mxli:&amp;nbsp;&lt;A class="link-titled" href="http://www.windscooting.com/softy/mxli.html" title="http://www.windscooting.com/softy/mxli.html"&gt;mxli - Marc's exquisite LPC ISP tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 20:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Using-ISP-Uart-Flash-Program/m-p/645831#M32663</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2016-12-28T20:20:42Z</dc:date>
    </item>
  </channel>
</rss>