<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Orange beetle symbol</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641972#M32642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I saw this settings, there were a lot of colored beetles. But all is unchecked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Nov 2016 11:13:24 GMT</pubDate>
    <dc:creator>pavelhudecek</dc:creator>
    <dc:date>2016-11-10T11:13:24Z</dc:date>
    <item>
      <title>Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641967#M32637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;At the left from the line number is&amp;nbsp;appeared symbol in the form of orange beetle.&lt;BR /&gt;If I move the mouse on this symbol, tooltip "Return has value, in function returning void" is shown.&lt;BR /&gt;Function is void, contains a&amp;nbsp;two returns and all are "return;"&lt;/P&gt;&lt;P&gt;The symbol is on the&amp;nbsp;first line after "{". This line is a&amp;nbsp;comment.&lt;/P&gt;&lt;P&gt;On the project icon, folder icon and source icon is the red "x" shown. At the right from the source box&amp;nbsp;the red rectangle is shown.&amp;nbsp;It is as if error occurred.&lt;/P&gt;&lt;P&gt;But the function has compiled properly and working properly.&lt;/P&gt;&lt;P&gt;All&amp;nbsp;these symbols never disappear.&lt;/P&gt;&lt;P&gt;It is started after I experimented with the "Customize perspective..."&lt;/P&gt;&lt;P&gt;How can I correct this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2016 13:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641967#M32637</guid>
      <dc:creator>pavelhudecek</dc:creator>
      <dc:date>2016-11-08T13:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641968#M32638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: The beetle is not orange. It is red, but sometimes is something yellow underneath.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2016 14:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641968#M32638</guid>
      <dc:creator>pavelhudecek</dc:creator>
      <dc:date>2016-11-08T14:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641969#M32639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would be helpful to see a screenshot of what you are trying to describe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's possible that you are seeing &amp;nbsp;the IDE's indexer and the compiler getting out of sync. &amp;nbsp;You could try right clicking on the project in the Project Explorer view, and selecting Index-&amp;gt; Rebuild&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, please confirm what version of LPCXpresso IDE are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2016 17:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641969#M32639</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-11-08T17:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641970#M32640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sounds like you have activated the Code Analysis features of LPCXpresso - it is trying to help you write better code! Open your project properties, on the left part of the dialog, select C/C++ General, and then the Code Analysis sub-section. You may have changed this setting for the project, or perhaps the whole workspace. (on this dialog, you will see all off the coloured beetles!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HTH&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2016 17:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641970#M32640</guid>
      <dc:creator>avt</dc:creator>
      <dc:date>2016-11-08T17:40:29Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641971#M32641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCXpresso v8.1.4 [Build 606] [2016-03-14]&amp;nbsp;&lt;/P&gt;&lt;P&gt;Project was imported from examples "Demos switch blinky",&amp;nbsp;it has been adapted to work with my board&amp;nbsp;and the original code was replaced by my code.&lt;/P&gt;&lt;P&gt;The problem looks like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="beetle.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9732i75FD5A604C1EB806/image-size/large?v=v2&amp;amp;px=999" role="button" title="beetle.png" alt="beetle.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After I try to clean up project and rebuild all, the beetle disappeared, but the "x" symbols remains. It happened on my home computer. Next I sync the Dropbox and go to work.&amp;nbsp;At a work computer the beetle appeared again, as shown in the screenshot.&lt;/P&gt;&lt;P&gt;After compilation this function properly works on my board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Nov 2016 11:09:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641971#M32641</guid>
      <dc:creator>pavelhudecek</dc:creator>
      <dc:date>2016-11-10T11:09:35Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641972#M32642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I saw this settings, there were a lot of colored beetles. But all is unchecked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Nov 2016 11:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641972#M32642</guid>
      <dc:creator>pavelhudecek</dc:creator>
      <dc:date>2016-11-10T11:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641973#M32643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: If I place /* at start and */ at end of this function, the beetle and "x" symbols stay. It's staying after the clean up, rebuild and reindex.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Beetle is not more bothered me, but the "x" is no different from the indicator of real error in code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2016 16:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641973#M32643</guid>
      <dc:creator>pavelhudecek</dc:creator>
      <dc:date>2016-11-11T16:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: Orange beetle symbol</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641974#M32644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did not know the hint from AVT, so I tried it and it works! I see&amp;nbsp;the beetle symbols. Are you sure you do not have this set in your project or workspace?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2016 17:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Orange-beetle-symbol/m-p/641974#M32644</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2016-11-11T17:54:06Z</dc:date>
    </item>
  </channel>
</rss>