<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Command line flash fails occasionally in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631567#M32530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That booting of the flasher seems to have been it. I had missed that documentation it completely... Thanks for the patience :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Sep 2016 15:52:01 GMT</pubDate>
    <dc:creator>kalleraiskila</dc:creator>
    <dc:date>2016-09-20T15:52:01Z</dc:date>
    <item>
      <title>Command line flash fails occasionally</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631565#M32528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having problems with flashing my target with a LPCLink2 programmer. Occasionally, when flashing from the command line, the flashing fails with &lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;1&lt;BR /&gt;Ni: LPCXpresso RedlinkMulti Driver v8.2 (Jun 30 2016 17:49:22 - crt_emu_cm_redlink build 723)&lt;BR /&gt;Pc: (&amp;nbsp; 0) Reading remote configuration&lt;BR /&gt;Pc: (&amp;nbsp; 5) Remote configuration complete&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(38). Invalid probe index.'&lt;BR /&gt;Nc: probe unbooted? no core 0?&lt;BR /&gt;Ed:02: Failed on connect: Ee(38). Invalid probe index.&lt;BR /&gt;Et:31: No connection to emulator device&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error might show up with one user account while it still works from another one, on the same machine,&amp;nbsp; with the same target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seem to not be able to repeat the problem when running from LPCXpresso GUI, but this might be just a statistical fluke. The failures seem to come "clustered", i.e. if it does not work once, it probably will not work if I retry, either. This makes figuring this out more difficult.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Launching the GUI is not a possible solution here, as I am building up an automated test setup. The command line I use for flashing is generated by the LPCXpresso GUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The machine is an Ubuntu 16.04, x86_64. LPCXpresso is version v8.2.0 [Build 647] [2016-07-18].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions on what I could try?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you in advance,&lt;/P&gt;&lt;P&gt;kalle&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 11:41:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631565#M32528</guid>
      <dc:creator>kalleraiskila</dc:creator>
      <dc:date>2016-09-19T11:41:13Z</dc:date>
    </item>
    <item>
      <title>Re: Command line flash fails occasionally</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631566#M32529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What actually is the command line that you are passing in? Are you passing in a probe index, if so, do you see the same issue if you remove this parameter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I presume you are booting the probe first, as per:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/388964"&gt;Booting LPC-Link2&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS : The following might be useful background if you haven't seen it already:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389139"&gt;https://community.nxp.com/thread/389139&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 07:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631566#M32529</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-09-20T07:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: Command line flash fails occasionally</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631567#M32530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That booting of the flasher seems to have been it. I had missed that documentation it completely... Thanks for the patience :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 15:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Command-line-flash-fails-occasionally/m-p/631567#M32530</guid>
      <dc:creator>kalleraiskila</dc:creator>
      <dc:date>2016-09-20T15:52:01Z</dc:date>
    </item>
  </channel>
</rss>