<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックUART for ISP</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630429#M32518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to program the on-chip flash of&amp;nbsp;LPC1313FBD48/01 device. I have connected the SWCLK and the SWDIO pins to the debug connector. The UART interface is connected to some other peripheral. I have some queries regarding the same:&lt;/P&gt;&lt;P&gt;Is it necessary to use ISP or IAP modes to program the flash or can it be done without that?&lt;/P&gt;&lt;P&gt;Also, if ISP mode is to be used, how is the UART interface to be used for this purpose?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Prachi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Mar 2017 11:01:04 GMT</pubDate>
    <dc:creator>prachipanse</dc:creator>
    <dc:date>2017-03-29T11:01:04Z</dc:date>
    <item>
      <title>UART for ISP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630429#M32518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to program the on-chip flash of&amp;nbsp;LPC1313FBD48/01 device. I have connected the SWCLK and the SWDIO pins to the debug connector. The UART interface is connected to some other peripheral. I have some queries regarding the same:&lt;/P&gt;&lt;P&gt;Is it necessary to use ISP or IAP modes to program the flash or can it be done without that?&lt;/P&gt;&lt;P&gt;Also, if ISP mode is to be used, how is the UART interface to be used for this purpose?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Prachi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 11:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630429#M32518</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-03-29T11:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: UART for ISP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630430#M32519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you have connected up the SWD signals, then you could debug using LPCXpresso IDE (or MCUXpresso IDE) plus a debug probe - such as LPC-Link2 :&amp;nbsp;&lt;A class="link-titled" href="http://www.nxp.com/lpclink2" title="http://www.nxp.com/lpclink2"&gt;LPC-Link2|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To make sure you have implement appropriate debug/reset circuitry, you might also want to check out the FAQ :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/388998"&gt;Design Considerations for Debug&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to program using ISP, then you will probably want to look at a utility such as FlashMagic :&amp;nbsp;&lt;A class="link-titled" href="http://www.flashmagictool.com" title="http://www.flashmagictool.com"&gt;Flash Magic - Welcome&lt;/A&gt;&amp;nbsp;(external site).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 10:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630430#M32519</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-03-30T10:57:54Z</dc:date>
    </item>
    <item>
      <title>Re: UART for ISP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630431#M32520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. This clarifies my query.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 11:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-for-ISP/m-p/630431#M32520</guid>
      <dc:creator>prachipanse</dc:creator>
      <dc:date>2017-03-30T11:01:01Z</dc:date>
    </item>
  </channel>
</rss>