<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックBuild Last Project Hotkey</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Build-Last-Project-Hotkey/m-p/617374#M32409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a possibility to setup a hotkey for the build "my project" [Debug] button?&lt;BR /&gt;I do not find this command in Window /Preferences /General /Keys&lt;/P&gt;&lt;P&gt;However there is a command "Build Project". This works only if I select first the project folder.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6772iF8ED8CDABFDC1CB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For debug I used the the command "Debug Last Launched".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6744i11069E7586E9D116/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I do&amp;nbsp;not want to start debuging if I only need to build the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a solution to add a hotkey to the Build "my project" button?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6822i20A515F314AB05E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 19:31:40 GMT</pubDate>
    <dc:creator>simonwyss</dc:creator>
    <dc:date>2017-04-17T19:31:40Z</dc:date>
    <item>
      <title>Build Last Project Hotkey</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Build-Last-Project-Hotkey/m-p/617374#M32409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a possibility to setup a hotkey for the build "my project" [Debug] button?&lt;BR /&gt;I do not find this command in Window /Preferences /General /Keys&lt;/P&gt;&lt;P&gt;However there is a command "Build Project". This works only if I select first the project folder.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6772iF8ED8CDABFDC1CB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For debug I used the the command "Debug Last Launched".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6744i11069E7586E9D116/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I do&amp;nbsp;not want to start debuging if I only need to build the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a solution to add a hotkey to the Build "my project" button?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6822i20A515F314AB05E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 19:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Build-Last-Project-Hotkey/m-p/617374#M32409</guid>
      <dc:creator>simonwyss</dc:creator>
      <dc:date>2017-04-17T19:31:40Z</dc:date>
    </item>
  </channel>
</rss>