<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPC Link, flash command line</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-flash-command-line/m-p/607545#M32296</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/388960"&gt;Booting LPC-Link&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also find this useful :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389139"&gt;Using the command line flash programming tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as installing a license&amp;nbsp;goes, the only way to activate&amp;nbsp;is via the IDE itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 10 Sep 2016 17:35:46 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-09-10T17:35:46Z</dc:date>
    <item>
      <title>LPC Link, flash command line</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-flash-command-line/m-p/607544#M32295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a LPC-Link that I'd like to use as command line programmer (Windows).&lt;/P&gt;&lt;P&gt;After IDE (LPC Xpresso) it initialize the boards, programming can be done by using a command line&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\nxp\LPCXpresso_8.0.0_526\lpcxpresso\bin\crt_emu_cm3_gen -flash-load-exec "test_project/Release/test_project.axf" -g -2 -vendor=NXP -pLPC824 -wire=hid -s3000 -flash-driver=LPC800_32.cfx -x D:/test_project/Release&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the question is how do I initialize the board like LPC Xpresso does?&lt;/P&gt;&lt;P&gt;Above line works until I unplug the USB from the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is very convenient for production programming, so don't need IDE anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, how can I provide the license in command line (a batch file probably) since I may use a computer that doesn't have a IDE installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Sep 2016 14:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-flash-command-line/m-p/607544#M32295</guid>
      <dc:creator>rianzu</dc:creator>
      <dc:date>2016-09-10T14:12:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Link, flash command line</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-flash-command-line/m-p/607545#M32296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/388960"&gt;Booting LPC-Link&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also find this useful :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389139"&gt;Using the command line flash programming tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as installing a license&amp;nbsp;goes, the only way to activate&amp;nbsp;is via the IDE itself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Sep 2016 17:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-flash-command-line/m-p/607545#M32296</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-09-10T17:35:46Z</dc:date>
    </item>
  </channel>
</rss>