<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: SWD configuration both devices not shown</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606090#M32271</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you! I put the jumper on JP5 and it worked after connecting the board with it (Windows first saw&amp;nbsp;a device "LPC", then "LPC-LINK2 CMSIS-DAP V5.173" after debugging).&lt;/P&gt;&lt;P&gt;But if I take off the jumper, I always go back with the old version of debug probe and it doesn't work anymore. (Windows sees it as "LPC-Link-II CMSIS-DAP" like before).&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the jumper JP5 on, I've tried in the IDE, "Boot Debug Probe", also "boot_lin2.cmd", "dfu-util.exe" in bin directory but it's like it doesn't keep in flash the updated new firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I not see, without the jumper on, the same device in Windows ? (&lt;SPAN&gt;"LPC-LINK2 CMSIS-DAP V5.173" &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Oct 2016 07:05:53 GMT</pubDate>
    <dc:creator>etienneschaeffe</dc:creator>
    <dc:date>2016-10-05T07:05:53Z</dc:date>
    <item>
      <title>SWD configuration both devices not shown</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606088#M32269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to run the multicore_binky example, but after debuging "multicore_m4master_blinky", I cannot debug "multicore_m0slave_blinky" in the same time. It says that "0 available SWD Devices detected." in SWD Configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, I could never choose between Cortex-M4 or Cortex-M0 in any project in the popup "SWD Configuration". It's like I had only one. So when I debug m4master, I don't see popup "SWD Configuration" and it works, then when I debug m0slave, I can see popup "SWD Configuration" but with no devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;LPCXpresso v8.2.2 [Build 650] with a OM13077.&lt;/P&gt;&lt;P&gt;And enulator is :&lt;/P&gt;&lt;P&gt;Name = LPC-Link-II CMSIS-DAP,&amp;nbsp;Serial number = A000000001,&amp;nbsp;Type = LinkServer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Etienne&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 16:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606088#M32269</guid>
      <dc:creator>etienneschaeffe</dc:creator>
      <dc:date>2016-10-04T16:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: SWD configuration both devices not shown</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606089#M32270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The most recent IDE versions will attempt to automatically detect and select the appropriate CPU within the multicore MCU for each project. Thus you may not even see the prompt asking you to select the right one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the IDE is not detecting a second core though, then I would recommend&lt;/P&gt;&lt;UL style="list-style-type: circle;"&gt;&lt;LI&gt;closing down all debug sessions&lt;/LI&gt;&lt;LI&gt;completely resetting your board,&lt;/LI&gt;&lt;LI&gt;and also ensuring that there are no rogue processes running called "arm-none-eabi-gdb", "crt_emu_cm_redlink" or "redlinkserv"&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It may also be a good idea to delete the .launch files within your master and slave projects, and also deleting the Debug/Release directories within them as well. Which will force the IDE to regenerate everything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an aside, if you haven't seen it already, I would recommend&amp;nbsp;reading:&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389074"&gt;LPC541xx Cortex-M4 / M0+ Multicore Applications&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I strongly suggest that you put a jumper on DFULink header (JP5 IIRC), so that the IDE can soft load the current debug probe firmware. From the details you provide, you are using a old version that has been preprogrammed into the probe's flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 16:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606089#M32270</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-10-04T16:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: SWD configuration both devices not shown</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606090#M32271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you! I put the jumper on JP5 and it worked after connecting the board with it (Windows first saw&amp;nbsp;a device "LPC", then "LPC-LINK2 CMSIS-DAP V5.173" after debugging).&lt;/P&gt;&lt;P&gt;But if I take off the jumper, I always go back with the old version of debug probe and it doesn't work anymore. (Windows sees it as "LPC-Link-II CMSIS-DAP" like before).&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the jumper JP5 on, I've tried in the IDE, "Boot Debug Probe", also "boot_lin2.cmd", "dfu-util.exe" in bin directory but it's like it doesn't keep in flash the updated new firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I not see, without the jumper on, the same device in Windows ? (&lt;SPAN&gt;"LPC-LINK2 CMSIS-DAP V5.173" &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 07:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606090#M32271</guid>
      <dc:creator>etienneschaeffe</dc:creator>
      <dc:date>2016-10-05T07:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: SWD configuration both devices not shown</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606091#M32272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you want to program the latest version of the probe firmware into the probe's flash - rather than letting LPCXpresso IDE soft load it, then you can do this using LPCScrypt. For more details see:&amp;nbsp;&lt;A href="https://community.nxp.com/message/630661"&gt;https://community.nxp.com/message/630661&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 10:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-configuration-both-devices-not-shown/m-p/606091#M32272</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-10-05T10:17:40Z</dc:date>
    </item>
  </channel>
</rss>