<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPCXpresso 54114 example code to write the script to specifically to RAM memory?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-54114-example-code-to-write-the-script-to/m-p/597480#M32201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The simplest way to do this is to user the Memory Configuration editor (as described in the LPCXpresso IDE User Manual) and delete all of the Flash memories, thus leaving just the RAM. The IDE will automatically create appropriate linker script and you will be able to download and debug your application in RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Apr 2017 16:05:38 GMT</pubDate>
    <dc:creator>thefallguy</dc:creator>
    <dc:date>2017-04-10T16:05:38Z</dc:date>
    <item>
      <title>LPCXpresso 54114 example code to write the script to specifically to RAM memory?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-54114-example-code-to-write-the-script-to/m-p/597479#M32200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;Could anyone provide me the sample code or the way to boot the codes/scripts directly into the RAM, rather than Flash Memory?&lt;/P&gt;&lt;P&gt;Demo code will be a great help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Himanshu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 11:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-54114-example-code-to-write-the-script-to/m-p/597479#M32200</guid>
      <dc:creator>himanshudoshi</dc:creator>
      <dc:date>2017-04-10T11:56:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso 54114 example code to write the script to specifically to RAM memory?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-54114-example-code-to-write-the-script-to/m-p/597480#M32201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The simplest way to do this is to user the Memory Configuration editor (as described in the LPCXpresso IDE User Manual) and delete all of the Flash memories, thus leaving just the RAM. The IDE will automatically create appropriate linker script and you will be able to download and debug your application in RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 16:05:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-54114-example-code-to-write-the-script-to/m-p/597480#M32201</guid>
      <dc:creator>thefallguy</dc:creator>
      <dc:date>2017-04-10T16:05:38Z</dc:date>
    </item>
  </channel>
</rss>