<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC2368 VIC</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2368-VIC/m-p/596933#M32041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nmariner on Thu Apr 24 09:48:27 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am quite new to expresso and am working on a LPC2368 device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When debugging my code I see that timer2 is not hitting an interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Timer2 itself is running but does not create an iterrupt. when looking at the VIC address in the peripherals monitor, I see only VICVectAddr0 to VICVectAddr15 are listed. Timer2 is on address 26.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any clues as to why the second half of the VIC vector addresses are not showing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One other strange issue, it seems that VICVectAddr14 is shown as adress 0xFFFFF108 and VICVectAddr15 is shown as 0xFFFFF10C which is mirroring VIC addresses 2 and 3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nigel.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:39:08 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:39:08Z</dc:date>
    <item>
      <title>LPC2368 VIC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2368-VIC/m-p/596933#M32041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nmariner on Thu Apr 24 09:48:27 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am quite new to expresso and am working on a LPC2368 device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When debugging my code I see that timer2 is not hitting an interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Timer2 itself is running but does not create an iterrupt. when looking at the VIC address in the peripherals monitor, I see only VICVectAddr0 to VICVectAddr15 are listed. Timer2 is on address 26.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any clues as to why the second half of the VIC vector addresses are not showing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;One other strange issue, it seems that VICVectAddr14 is shown as adress 0xFFFFF108 and VICVectAddr15 is shown as 0xFFFFF10C which is mirroring VIC addresses 2 and 3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nigel.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC2368-VIC/m-p/596933#M32041</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:39:08Z</dc:date>
    </item>
  </channel>
</rss>