<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: 1769 pwm</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596898#M32017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by 1769user on Wed Jan 30 07:34:21 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried searching but couldn't find anything useful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For example, there is a problem with PWMLER. It seems that this is only reset to zero by a match if bit 0( for MR0) is set? If I set the bits for MR5 and MR6, these remain set. If I set bit 0, all the bits are reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Trial and error is a very slow process.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:36:16 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:36:16Z</dc:date>
    <item>
      <title>1769 pwm</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596896#M32015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by 1769user on Wed Jan 30 02:31:16 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am having problems getting this to generate a couple of PWM outputs. Has anyone a comprehensive list of the registers that need to be initialised? Better still would be a commented example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596896#M32015</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 pwm</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596897#M32016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Jan 30 02:56:17 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: 1769user&lt;/STRONG&gt;&lt;BR /&gt;Better still would be a commented example.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;:confused:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There are several threads about LPC1769 PWM like:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?p=16360&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A simple search could help :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596897#M32016</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: 1769 pwm</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596898#M32017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by 1769user on Wed Jan 30 07:34:21 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried searching but couldn't find anything useful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For example, there is a problem with PWMLER. It seems that this is only reset to zero by a match if bit 0( for MR0) is set? If I set the bits for MR5 and MR6, these remain set. If I set bit 0, all the bits are reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Trial and error is a very slow process.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/1769-pwm/m-p/596898#M32017</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:36:16Z</dc:date>
    </item>
  </channel>
</rss>