<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックCreating binary resource-only image</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595589#M31450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wdawson61 on Thu Sep 08 18:37:42 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all.&amp;nbsp; I have some binary data that I want to program at a fixed address in flash.&amp;nbsp; The data is contained in c source files that were part of my main project.&amp;nbsp; I now want to move them out of the main source project and create a new project that has only these tables.&amp;nbsp; I then want to program them at a fixed location in flash say 0x20000.&amp;nbsp; I'm having a hard time figuring out how to create a resource-only project in lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm mainly doing this to overcome the 128k max size limit.&amp;nbsp; I've purchased the code-red nxp version with a 256K download limit but don't really want to shift from Linux to Windows at this late stage in the project, so I'm trying to find a workaround for this limitation.&amp;nbsp; I have external scripts / linux utilities as build steps that I'd prefer not move to Windoze right yet.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone done anything like this or can anyone recommend a solution?&amp;nbsp; I've tried using ld then objcopy but I can't seem to get ld to create a pure binary file without a bunch of symbol table stuff even with -S (and -s).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas are greatly appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-Wade&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:33:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:33:47Z</dc:date>
    <item>
      <title>Creating binary resource-only image</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595589#M31450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wdawson61 on Thu Sep 08 18:37:42 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all.&amp;nbsp; I have some binary data that I want to program at a fixed address in flash.&amp;nbsp; The data is contained in c source files that were part of my main project.&amp;nbsp; I now want to move them out of the main source project and create a new project that has only these tables.&amp;nbsp; I then want to program them at a fixed location in flash say 0x20000.&amp;nbsp; I'm having a hard time figuring out how to create a resource-only project in lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm mainly doing this to overcome the 128k max size limit.&amp;nbsp; I've purchased the code-red nxp version with a 256K download limit but don't really want to shift from Linux to Windows at this late stage in the project, so I'm trying to find a workaround for this limitation.&amp;nbsp; I have external scripts / linux utilities as build steps that I'd prefer not move to Windoze right yet.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone done anything like this or can anyone recommend a solution?&amp;nbsp; I've tried using ld then objcopy but I can't seem to get ld to create a pure binary file without a bunch of symbol table stuff even with -S (and -s).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas are greatly appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-Wade&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595589#M31450</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: Creating binary resource-only image</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595590#M31451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Fri Sep 09 08:49:40 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: wdawson61&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp; I've purchased the code-red nxp version with a 256K download limit but don't really want to shift from Linux to Windows at this late stage in the project, so I'm trying to find a workaround for this limitation.&amp;nbsp; I have external scripts / linux utilities as build steps that I'd prefer not move to Windoze right yet.&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought Code Red had a Linux version of Red Suite 4. Maybe you should check with them.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595590#M31451</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: Creating binary resource-only image</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595591#M31452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by atomicdog on Fri Sep 09 11:42:11 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems like you could just use the section attribute on the data in the new project to have the data put in the location you want.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Creating-binary-resource-only-image/m-p/595591#M31452</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:48Z</dc:date>
    </item>
  </channel>
</rss>