<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Can't suspend or terminate debugger</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594960#M31190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Seba on Wed Sep 18 04:40:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I faced the same problem. Hardware: LPCXpresso LPC1347 board (Embedded Artists) - no modifications. I've tried many projects starting from simple increment variable program and FreeRTOS based one. All applications work properly on target. I can connect to HW, load program to flash, set breakpoints, see variable/register values, run, step over, step into, restart - all these actions work properly. The problem is when I try to make any action (eg Suspend or set breakpoint) while program is running. Any action cause target disconnection. So I can't Suspend running program. My workaround is to set breakpoint in GPIO interrupt routine and press button every time I want to Suspend.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:55:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:55:26Z</dc:date>
    <item>
      <title>Can't suspend or terminate debugger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594956#M31186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by markustmaier on Tue Aug 27 12:00:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm new to microcontroller and have a problem with debugging in LPCxpresso:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't suspend or terminate the debugger. If I click the button nothing happens. I can step in or step over and I can set breakpoints. But suspend and terminate does not work. The only way to stop it is to pull the usb cable of LPC-Link (with errors).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tested with LPCXpresso v5.1.2_2065 and LPCXpresso v5.2.6_2137. Target is LPC1769 from the Embedded Artists Board with LPC-Link. The Embedded Artists Base Board is not connected. System is Win7 x64. I've also tested several included projects like "demo" or "uart2".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas why this does not work and what I can do to get it working?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Markus&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594956#M31186</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: Can't suspend or terminate debugger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594957#M31187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 27 13:00:49 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Please describe exactly which buttons you are pressing and when, and describe what is happening. Please attach screenshots if you can.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have never heard of this problem, so I think it is something you are misunderstanding.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594957#M31187</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: Can't suspend or terminate debugger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594958#M31188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by markustmaier on Tue Aug 27 13:17:57 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for the fast response.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Here is what I'm doing:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Start LPCxpresso&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Connect LPC-Link with LPC1769 directly to USB Port (no Hub)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Select Project "Demo" in Project Explorer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4. Clean "Demo" (Quickstart Panel)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5. Debug "Demo" (Quickstart Panel) -&amp;gt; Wait for download to target&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;6. Debugger is starting at first line of main() (see screenshot 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;7. If I press "Resume" (see screenshot 2) the controller starts working&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;8. If I now press "Suspend" nothing happens. I can't press "Step over" or "Step into" anymore. The Suspend and the Resume button is gray. I can only press terminate. I know that usually the processor stop and the debug windows highlights the acutal line. I can't do anything to stop the controller. If I press Terminate also nothing happens. (see screenshot 3)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alternative:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Step 1 to 6 above&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;7. I press "Step over" or "Step into" and every thing is fine. But again I can't terminate the session. If I press the button nothing happens.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can there something be wrong with my debug settings? I used LPCxpresso about one year ago with an LPC1343 an no problems. Now I installed the new version and imported the example projects into a new workspace.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594958#M31188</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can't suspend or terminate debugger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594959#M31189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 27 23:48:00 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this a standard board or a custom board (one of your own design)? If it is a custom board, please try with a standard board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, please try debugging a simple C application created with the wizard. try debugging it several times.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please report back your results.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I am thinking of two possibilities&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. If it is your own board, there is a problem with the debug circuit&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;2. Your application is putting the target into a mode where the debugger cannot gain access. See &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsupport.code-red-tech.com%2FCodeRedWiki%2FDebugAccessChip" rel="nofollow" target="_blank"&gt;http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594959#M31189</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can't suspend or terminate debugger</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594960#M31190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Seba on Wed Sep 18 04:40:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I faced the same problem. Hardware: LPCXpresso LPC1347 board (Embedded Artists) - no modifications. I've tried many projects starting from simple increment variable program and FreeRTOS based one. All applications work properly on target. I can connect to HW, load program to flash, set breakpoints, see variable/register values, run, step over, step into, restart - all these actions work properly. The problem is when I try to make any action (eg Suspend or set breakpoint) while program is running. Any action cause target disconnection. So I can't Suspend running program. My workaround is to set breakpoint in GPIO interrupt routine and press button every time I want to Suspend.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Can-t-suspend-or-terminate-debugger/m-p/594960#M31190</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:55:26Z</dc:date>
    </item>
  </channel>
</rss>