<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックProblem on USBHID example code in LPC1343</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-on-USBHID-example-code-in-LPC1343/m-p/532513#M3110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wsyuen on Thu Feb 10 22:01:36 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I modified the USBHID sample as a USB keyboard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It works when I plug in the PC when the PC is turned ON.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, if I plug in the PC and then turn ON the PC, it can't recognise it as a USB keyboard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it anything need to do with the code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the following functions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USBIOClkConfig();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USB_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USB_Connect(TRUE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and I haven't use the Soft Connect function, D+ is always pull-high with a 1.5k resistor.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:57:09 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:57:09Z</dc:date>
    <item>
      <title>Problem on USBHID example code in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-on-USBHID-example-code-in-LPC1343/m-p/532513#M3110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wsyuen on Thu Feb 10 22:01:36 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I modified the USBHID sample as a USB keyboard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It works when I plug in the PC when the PC is turned ON.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However, if I plug in the PC and then turn ON the PC, it can't recognise it as a USB keyboard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it anything need to do with the code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the following functions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USBIOClkConfig();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USB_Init();&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; USB_Connect(TRUE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and I haven't use the Soft Connect function, D+ is always pull-high with a 1.5k resistor.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-on-USBHID-example-code-in-LPC1343/m-p/532513#M3110</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on USBHID example code in LPC1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-on-USBHID-example-code-in-LPC1343/m-p/532514#M3111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Luis Digital on Fri Feb 11 06:20:25 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe you need to activate in the BIOS Emulator keyboard / mouse USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;support.microsoft.com/kb/310923&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-on-USBHID-example-code-in-LPC1343/m-p/532514#M3111</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:57:10Z</dc:date>
    </item>
  </channel>
</rss>