<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Execution time for LPC1317 Set instruction in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594401#M30944</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Deepak Bansal on Tue Sep 25 22:00:24 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1. I am running CPU at 72Mhz &amp;amp; same clock given to GPIO with divide by 1 clock divider.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So GPIO clock is also 72Mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I use &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO-&amp;gt;SET[0] = 0x04; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is taking greater than 70 nsec time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should't it be lesser than that, as it is single cycle inst.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:33:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:33:54Z</dc:date>
    <item>
      <title>Execution time for LPC1317 Set instruction</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594401#M30944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Deepak Bansal on Tue Sep 25 22:00:24 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1. I am running CPU at 72Mhz &amp;amp; same clock given to GPIO with divide by 1 clock divider.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So GPIO clock is also 72Mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I use &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO-&amp;gt;SET[0] = 0x04; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is taking greater than 70 nsec time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Should't it be lesser than that, as it is single cycle inst.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594401#M30944</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: Execution time for LPC1317 Set instruction</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594402#M30945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Tue Sep 25 23:52:40 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1. look at the code the compiler generated - it will be more than one instruction&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. It will be much worse when compiling for Debug. If you want to see smaller/faster code, compile for Release.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. If you are really worried about performance in critical sections, write in assembler.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See the Code Red faq on optimization&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/CompilerOptimization&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594402#M30945</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: Execution time for LPC1317 Set instruction</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594403#M30946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Wed Sep 26 06:51:23 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you waant to run at full clock speed you must run from cache or RAM.&amp;nbsp;&amp;nbsp; Flash memory imposes wait states.&amp;nbsp;&amp;nbsp; If your loop is very small then it might fit in cache.&amp;nbsp;&amp;nbsp; For cache, address alignment and size matter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If that won't work, then you can move the critical code into RAM and run it there.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RAM runs without wait states.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There are threads that have discussed these issues.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594403#M30946</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Execution time for LPC1317 Set instruction</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594404#M30947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Deepak Bansal on Fri Sep 28 22:08:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have checked its disassembly, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO-&amp;gt;SET[tft_rst_port] = tft_rst_pin;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00000DAE F44F4180&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#0x4000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00000DB2 4895&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[pc,#596]&amp;nbsp; ; @0x00001008&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00000DB4 3080&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADDS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,r0,#0x80&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x00000DB6 6041&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,[r0,#0x04]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Single instruction SET, has 4 cycle. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any single cycle inst to set &amp;amp; clr pin, in C.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How could I add assembly in C.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using Keil V 4.54.0.0&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594404#M30947</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Execution time for LPC1317 Set instruction</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594405#M30948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by daniel.widyanto on Tue Oct 09 21:22:03 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ask Keil question in Keil forum (&lt;/SPAN&gt;&lt;A href="http://http://www.keil.com/forum/"&gt;http://www.keil.com/forum/&lt;/A&gt;&lt;SPAN&gt;). This is LPCXpresso forum&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Execution-time-for-LPC1317-Set-instruction/m-p/594405#M30948</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:33:57Z</dc:date>
    </item>
  </channel>
</rss>