<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wi Fi Module to use with LPCXpresso 1343 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Wi-Fi-Module-to-use-with-LPCXpresso-1343/m-p/594108#M30781</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by oingo456 on Fri Jan 28 10:46:23 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Red Pine has some modules that have their own internal TCP/IP stack.&amp;nbsp; You can just hook them up over a serial port and use some escape codes to set up the wireless channel, etc.&amp;nbsp; Might be easier.&amp;nbsp; Data throughput is limited by the serial connection though.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; They also have some that don't have a stack, but the sample drivers might be for windows CE or something.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:52:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:52:39Z</dc:date>
    <item>
      <title>Wi Fi Module to use with LPCXpresso 1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Wi-Fi-Module-to-use-with-LPCXpresso-1343/m-p/594107#M30780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tomatongo on Thu Jan 27 17:50:35 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We are researching a Indoor Location System (Like GPS but inside buildings) and trying to scan available Networks and it's RSSI for pattern matching.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone has done some work with connecting an LPC1343 to a Wi Fi Module? I think we wont be needing TCP/IP Stack (only Phy) so LPC1343 will be enough to do the trick. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas or suggestions of chips to start working with?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance!!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tom.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Wi-Fi-Module-to-use-with-LPCXpresso-1343/m-p/594107#M30780</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: Wi Fi Module to use with LPCXpresso 1343</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Wi-Fi-Module-to-use-with-LPCXpresso-1343/m-p/594108#M30781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by oingo456 on Fri Jan 28 10:46:23 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Red Pine has some modules that have their own internal TCP/IP stack.&amp;nbsp; You can just hook them up over a serial port and use some escape codes to set up the wireless channel, etc.&amp;nbsp; Might be easier.&amp;nbsp; Data throughput is limited by the serial connection though.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; They also have some that don't have a stack, but the sample drivers might be for windows CE or something.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:52:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Wi-Fi-Module-to-use-with-LPCXpresso-1343/m-p/594108#M30781</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:52:39Z</dc:date>
    </item>
  </channel>
</rss>