<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPC1768 input pin voltage is low with internal pull-up</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593712#M30576</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ppescher on Wed Nov 23 07:41:51 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, I do understand that internal pull-ups are there to prevent unconfigured pins to float, and this is standard practice in every uC I know about. But this is the first time I come across an issue like this, that an internally pulled-up pin barely reaches the VIH. This is weird, if not crazy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The real problem here is that this kind of behavior is not documented. I read the datasheet, page 52 figure 13, and I see that with 2.3V input voltage I should have a pull-up current of 30uA. Where does that current flow if I leave the input pin unconnected? Or should I assume it flows in the &amp;gt;1M Ohm load of my instruments, giving me more than 30V!? That pull-up current is way much lower, let's say 2uA, which is well under the minimum pull-up current of 15uA documented in the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just want official documentation about internal pull-ups which is correct, so I can design properly. I can't make assumptions based on my or other people's measures. For instance, what happens to measured values at -40°C or 85°C?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:31:27 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:31:27Z</dc:date>
    <item>
      <title>LPC1768 input pin voltage is low with internal pull-up</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593709#M30573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ppescher on Wed Nov 23 04:39:01 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen this post:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?t=381&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I confirm that after reset pins are configured as inputs with internal pull-up and voltage is measured at around 2.3V - 2.4V, with a VDD=3.3V (pin unloaded). This is too close to the VIH threshold 0.7*VDD = 2.31V to be really useful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The datasheet does not specify that behavior, so I would like to know some official word from NXP about this, or someone that points me to official documentation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As it is, the internal pull-up doesn't seem useful. Is the input voltage with internal pull-up guaranteed to be higher than VIH in all the operating range? Are the electrical characteristics reported in the datasheet correct? Because it doesn't seem so.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I definitely agree with user &lt;/SPAN&gt;&lt;A href="http://http://knowledgebase.nxp.com/member.php?u=633"&gt;dpalchak&lt;/A&gt;&lt;SPAN&gt; about this issue: it does matter!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I opened a new thread to give it more attention.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593709#M30573</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 input pin voltage is low with internal pull-up</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593710#M30574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Nov 23 06:51:53 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;A few unofficial notes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#1 Older datasheets shows VIH HIGH-level input voltage: 2V :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#2 Measuring input voltages while input is switching high/low shows more friendly values about 1.6V and 1.2V :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#3 If you don't trust internal pullups, listen to your hardware engineer and use external pullups :eek:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593710#M30574</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 input pin voltage is low with internal pull-up</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593711#M30575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Wed Nov 23 07:20:44 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;IMHO the internal pull ups are just there to make sure your unused input pins are not floating. You should always use external pull ups when using input pins.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is how I look at this from a hardware engineer point of view. The internal pull ups are just too weak to be really useful in an application - the slightest glitch on a nearby track on the PCB may result in spurious signals. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I agree that this kind of limits the use of the internal pull up/down setting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[INDENT]Rob&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/INDENT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593711#M30575</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 input pin voltage is low with internal pull-up</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593712#M30576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ppescher on Wed Nov 23 07:41:51 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, I do understand that internal pull-ups are there to prevent unconfigured pins to float, and this is standard practice in every uC I know about. But this is the first time I come across an issue like this, that an internally pulled-up pin barely reaches the VIH. This is weird, if not crazy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The real problem here is that this kind of behavior is not documented. I read the datasheet, page 52 figure 13, and I see that with 2.3V input voltage I should have a pull-up current of 30uA. Where does that current flow if I leave the input pin unconnected? Or should I assume it flows in the &amp;gt;1M Ohm load of my instruments, giving me more than 30V!? That pull-up current is way much lower, let's say 2uA, which is well under the minimum pull-up current of 15uA documented in the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just want official documentation about internal pull-ups which is correct, so I can design properly. I can't make assumptions based on my or other people's measures. For instance, what happens to measured values at -40°C or 85°C?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593712#M30576</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 input pin voltage is low with internal pull-up</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593713#M30577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ToBeFrank on Sat Nov 26 21:08:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is just an FYI for anyone who finds this thread while searching, this appears to be device specific. This is what the 11XX manual says:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;If the pull-up resistor is enabled (default), all non-I2C pins are pulled up to 2.6 V for LPC111x/101/201/301 parts and pulled up to 3.3 V for LPC11Cxx parts and LPC111x/102/202/302 (VDD = 3.3 V).&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have verified that the LPC11C24 does indeed pull-up to 3.3V with the internal pull-ups.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-input-pin-voltage-is-low-with-internal-pull-up/m-p/593713#M30577</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:28Z</dc:date>
    </item>
  </channel>
</rss>