<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: RedProbe+ Error</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593314#M30401</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by liza on Tue Apr 10 04:34:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am experiencing a similar, but not exactly the same situation (resolved but solution is not consistent and even when worked then in the console window some errors popped up):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- when I build and debug adc_buzzer example from&amp;nbsp; examples.lpc17xx.new.zip then code builds and is downloads to my own target board and debugging works fine ALWAYS.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- but when I switch (within the same workspace) to my own project (same micro as in the above), code builds ok but when I try to start debug session then I get all kind of errors - almost always different one (in between attempts I unplugged the USB / Xpresso board etc in order to fix the problem): &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Target error from Commit [COLOR=Blue]Flash write: Et: Flash driver not ready.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Then at the next attempt : [COLOR=Blue]Failed on connect : EM(04). Can not provide power to DAP bus.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. then another one : &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]error :&amp;nbsp; No emulator/board available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This could be because it is unpowered, disconnected or already in use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I restarted LPCXPRESSO IDE and saw briefly this in 'console window' (btw : WHY IS ALL Info DISAPPEARING from there ? It would be very useful if it stayed !): [INDENT][COLOR=Blue]set remotetimeout 60000[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]info program[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Debugging a target over a serial line.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Program stopped at 0x4f0.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Type "info stack" or "info registers" for more information.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]set mem inaccessible-by-default off[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]mon ondisconnect cont[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]set arm force-mode thumb[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/INDENT]Whatever all that means somehow it managed to load the code and when I kicked the debugger (F8) my appication on my target board became alive and seems working fine. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am really scared to turn anything off at the end of today ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There probably must be some timeout or hidden setting(s) that causes it. Searched the net - no luck. But whatever it is - with 3 different errors above may be my pseudo fix of restarting the LPCXPRESSO IDE will help somebody with similar problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I run Win XP SP3.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:53:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:53:57Z</dc:date>
    <item>
      <title>RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593306#M30393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tom84 on Mon Mar 19 06:57:08 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCxpresso, a RedProbe+ and the Keil Evaluationboard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But i get an Error: &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][COLOR=#008000][SIZE=2][COLOR=#008000]Invalid LPC1768 Part ID: 0x25013F37&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Known LPC1768 ID(s): 0x00013F37, 0x26013F37, 0x26113F3[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][COLOR=#ff0000][SIZE=2][COLOR=#ff0000]03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part[/COLOR][/SIZE][/COLOR][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=#ff0000][COLOR=#ff0000][COLOR=black]What settings have to be changed?[/COLOR]&amp;nbsp; [COLOR=black]Or where can i change the chip, cause im using the lpc1758. I don't think that the problem is the 1768, but i have no clue whats wrong.....[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/COLOR]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593306#M30393</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593307#M30394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Mon Mar 19 07:02:16 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you try reading the FAQ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Especially:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593307#M30394</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:53Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593308#M30395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tom84 on Mon Mar 19 07:11:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I changed the MCU, know i can debug, but i can't flash :-(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The Error is: [COLOR=red]Connect to emulator or board:[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=red] No emulator/board available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This could be because it is unpowered, disconnected or already in use[/COLOR]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593308#M30395</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593309#M30396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Mon Mar 19 07:33:06 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps that is because your target is [COLOR=red]unpowered, disconnected or already in use[/COLOR]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593309#M30396</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593310#M30397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tom84 on Mon Mar 19 07:42:16 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for such a useless comment!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's powered, connected and not in use!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I erased the Chip via Keil uvision4, bur get still the sam eerror! &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And if i use the Keil Debugger and IDE, it works fine...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593310#M30397</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593311#M30398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tom84 on Mon Mar 19 08:01:50 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Problem solved, it works!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593311#M30398</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593312#M30399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Mon Mar 19 09:13:44 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;...so what was the problem? It might be helpful to others.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593312#M30399</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593313#M30400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tom84 on Tue Mar 20 00:54:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I just don't know :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;turned the computer off and back on....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593313#M30400</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:57Z</dc:date>
    </item>
    <item>
      <title>Re: RedProbe+ Error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593314#M30401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by liza on Tue Apr 10 04:34:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am experiencing a similar, but not exactly the same situation (resolved but solution is not consistent and even when worked then in the console window some errors popped up):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- when I build and debug adc_buzzer example from&amp;nbsp; examples.lpc17xx.new.zip then code builds and is downloads to my own target board and debugging works fine ALWAYS.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- but when I switch (within the same workspace) to my own project (same micro as in the above), code builds ok but when I try to start debug session then I get all kind of errors - almost always different one (in between attempts I unplugged the USB / Xpresso board etc in order to fix the problem): &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Target error from Commit [COLOR=Blue]Flash write: Et: Flash driver not ready.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Then at the next attempt : [COLOR=Blue]Failed on connect : EM(04). Can not provide power to DAP bus.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. then another one : &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]error :&amp;nbsp; No emulator/board available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This could be because it is unpowered, disconnected or already in use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I restarted LPCXPRESSO IDE and saw briefly this in 'console window' (btw : WHY IS ALL Info DISAPPEARING from there ? It would be very useful if it stayed !): [INDENT][COLOR=Blue]set remotetimeout 60000[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]info program[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Debugging a target over a serial line.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Program stopped at 0x4f0.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]Type "info stack" or "info registers" for more information.[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]set mem inaccessible-by-default off[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]mon ondisconnect cont[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[COLOR=Blue]set arm force-mode thumb[/COLOR]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/INDENT]Whatever all that means somehow it managed to load the code and when I kicked the debugger (F8) my appication on my target board became alive and seems working fine. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am really scared to turn anything off at the end of today ... &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There probably must be some timeout or hidden setting(s) that causes it. Searched the net - no luck. But whatever it is - with 3 different errors above may be my pseudo fix of restarting the LPCXPRESSO IDE will help somebody with similar problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I run Win XP SP3.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/RedProbe-Error/m-p/593314#M30401</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:57Z</dc:date>
    </item>
  </channel>
</rss>