<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP: Multiplexed I/O Pins: Documentation Request in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/NXP-Multiplexed-I-O-Pins-Documentation-Request/m-p/593246#M30373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Nov 02 14:07:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I appears (from various postings and UM's and personal experience) that at least some of the port&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;setup bits (pull up/down, hysteresis, slew etc. etc. are acted upon even when an alternate function&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(i.e not GPIO) is selected for the pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For those of us who came to embedded design via the software route, can NXP publish &lt;/SPAN&gt;&lt;I&gt;MCU agnsotic&lt;/I&gt;&lt;BR /&gt;&lt;SPAN&gt;details of the best practice when setting up I/O pins (i.e. what pull up/down, fast slew, hysteresis, glitch&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;filter, open-drain, invert, etc.) should be used when selecting various I/O functionality such as:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SPI, I2C, SD card, LCD, External Memory Contoller Address/Data/Control, CAN, UART, Ethernet, USB,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ADC, DAC, I2S, and other built in peripherals in the various MCUs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Manuals say what can be set, but not when and why!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;For widest availability, this should be first an App Note, and second an lpcware blog.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And we should be discussing I/O pin capabilities without the confusion of actual IO register details&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of reference to LPC Open or other headers -- The actual mechanics of implementing the settings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;vary wildy amongst the MCU families and specific code examples will only confuse users who favour&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;devices from different families.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Strictly speaking, this is not NXP's problem; but surely helping newcommers to create sucessful and robust&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;designs will boost NXP's image and reputation, and increase chip sales in the hobyist arena.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:29:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:29:59Z</dc:date>
    <item>
      <title>NXP: Multiplexed I/O Pins: Documentation Request</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/NXP-Multiplexed-I-O-Pins-Documentation-Request/m-p/593246#M30373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Nov 02 14:07:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I appears (from various postings and UM's and personal experience) that at least some of the port&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;setup bits (pull up/down, hysteresis, slew etc. etc. are acted upon even when an alternate function&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(i.e not GPIO) is selected for the pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For those of us who came to embedded design via the software route, can NXP publish &lt;/SPAN&gt;&lt;I&gt;MCU agnsotic&lt;/I&gt;&lt;BR /&gt;&lt;SPAN&gt;details of the best practice when setting up I/O pins (i.e. what pull up/down, fast slew, hysteresis, glitch&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;filter, open-drain, invert, etc.) should be used when selecting various I/O functionality such as:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;SPI, I2C, SD card, LCD, External Memory Contoller Address/Data/Control, CAN, UART, Ethernet, USB,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ADC, DAC, I2S, and other built in peripherals in the various MCUs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Manuals say what can be set, but not when and why!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;For widest availability, this should be first an App Note, and second an lpcware blog.&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And we should be discussing I/O pin capabilities without the confusion of actual IO register details&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of reference to LPC Open or other headers -- The actual mechanics of implementing the settings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;vary wildy amongst the MCU families and specific code examples will only confuse users who favour&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;devices from different families.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Strictly speaking, this is not NXP's problem; but surely helping newcommers to create sucessful and robust&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;designs will boost NXP's image and reputation, and increase chip sales in the hobyist arena.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/NXP-Multiplexed-I-O-Pins-Documentation-Request/m-p/593246#M30373</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: NXP: Multiplexed I/O Pins: Documentation Request</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/NXP-Multiplexed-I-O-Pins-Documentation-Request/m-p/593247#M30374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Tue Nov 25 10:02:16 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/NXP-Multiplexed-I-O-Pins-Documentation-Request/m-p/593247#M30374</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:30:00Z</dc:date>
    </item>
  </channel>
</rss>