<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 11c24 UART Problem in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593188#M30346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nfs2k on Wed Mar 21 04:23:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i got an lpc11c24 evaluation board. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i connected an USB to RS232/TTL/485 adapter to the RX and TX of the EV-Board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from putty i was able to send eg. an 'a' and the lpc did an echo so i got back the 'a'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;now i connected the RX and TX to another converter which does 232 to 485 . on it there is a MAX232N and the MAX489CPD. Now if i send some data from the board into bus for example an 'a' another mcu gets somthing else but no 'a' . &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;anyone knows where the problem could be ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfs2k&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:53:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:53:07Z</dc:date>
    <item>
      <title>11c24 UART Problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593188#M30346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nfs2k on Wed Mar 21 04:23:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i got an lpc11c24 evaluation board. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i connected an USB to RS232/TTL/485 adapter to the RX and TX of the EV-Board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from putty i was able to send eg. an 'a' and the lpc did an echo so i got back the 'a'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;now i connected the RX and TX to another converter which does 232 to 485 . on it there is a MAX232N and the MAX489CPD. Now if i send some data from the board into bus for example an 'a' another mcu gets somthing else but no 'a' . &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;anyone knows where the problem could be ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfs2k&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593188#M30346</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:07Z</dc:date>
    </item>
    <item>
      <title>Re: 11c24 UART Problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593189#M30347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Mar 21 04:42:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: nfs2k&lt;/STRONG&gt;&lt;BR /&gt;...now i connected the RX and TX to another converter which does 232 to 485 .&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So you connected 3.3V TTL of LPC11C24 to RS232 input :confused:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593189#M30347</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:08Z</dc:date>
    </item>
    <item>
      <title>Re: 11c24 UART Problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593190#M30348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nfs2k on Wed Mar 21 06:51:47 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;if i connect RX and TX to pins 9 &amp;amp; 10 of MAX232N which are for TTL use i can´t read nor write ... if i connect to pin 7 &amp;amp; 8 i can communicate but there are wrong characters... or fo i have the problem with the Voltage differences ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/11c24-UART-Problem/m-p/593190#M30348</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:09Z</dc:date>
    </item>
  </channel>
</rss>