<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCXpresso with LPC-Link2 jtag in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593166#M30342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Thu Aug 06 01:39:45 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear Support, thanks for the hints.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've moved to Windows8 with the latest LPCXpresso version 7.9.0 (see attached picture LPCXpresso_1.JPG).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm always using lpc4088-quickstart-board with LPC-Link 2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I try to download and debug the software (by means "Debug 'test1' button), the "LPC based USB device" disappears from the device manager and LPCXpresso stops at 95% (see attached picture LPCXpresso_2.JPG).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you have any idea about this issue?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:31:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:31:49Z</dc:date>
    <item>
      <title>LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593160#M30336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Wed Aug 05 05:19:56 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso (v7.0.2 on windows XP) with "LPC4088 QuickStart Board".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In order to download and debug the firmware, I'm trying to use the "LPC-Link 2" debug adapter.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the J8 connector on the "LPC-Link 2" connected to the J7 connector on the "LPC4088 QuickStart Board".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I try do debug the project, LPCXpresso doesn't recognize the "LPC-Link 2" debugger (see attached picture).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The hardware manager shows that the "LPC-Link 2" is correctly installed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you have any idea in order to fix this issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks in advance&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alberto&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593160#M30336</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593161#M30337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 05:49:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso 7.0.2 does not support CMSIS-DAP. If you must use that version of LPCXpresso, you must let it soft-boot LPC-Link2 by removing J2.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593161#M30337</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593162#M30338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Wed Aug 05 06:58:31 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Support,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for the hint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'd like to use LPCXpresso 7.0.2 because of I'm using windows XP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried with JP2 removed on LPC-Link2 (see attached picture), but the result is the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any other suggestion?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alberto&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593162#M30338</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593163#M30339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 07:08:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, that should have been JP1. See&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Flpc-link2-support" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-support&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593163#M30339</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593164#M30340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Wed Aug 05 07:28:40 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Don't worry, but I've already tried different combination of JP1 and JP2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you tell me the right combination of JP1 and JP2 on LPC-Link2 and JP3 on LPC4088 (for example JP1 removed, JP2 inserted and JP3 removed)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;About the LPCXpresso there is some setting to do? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For example I've seen that is possible to select the emulator and the debug template (see attached picture)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593164#M30340</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593165#M30341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 08:49:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You need to soft-boot LPC-Link2 with the Redlink image. This is done automatically by LPCXpresso 7.0.2 when&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- JP1 is removed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- you power-cycle LPC-Link2 after removing JP1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;JP2 is supplying target power and should NOT be inserted if the target is already being supplied with power.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso will automatically detect the Debug Adapter. If the project has been configured to use CMSIS-DAP, you can just "Search for any enabled emulator" when prompted the configuration will be reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As 7.0.2 is obsolete, and we do not have Windows XP here, we will be unable to provide any further assistance on this topic.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593165#M30341</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593166#M30342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Thu Aug 06 01:39:45 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear Support, thanks for the hints.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've moved to Windows8 with the latest LPCXpresso version 7.9.0 (see attached picture LPCXpresso_1.JPG).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm always using lpc4088-quickstart-board with LPC-Link 2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I try to download and debug the software (by means "Debug 'test1' button), the "LPC based USB device" disappears from the device manager and LPCXpresso stops at 95% (see attached picture LPCXpresso_2.JPG).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you have any idea about this issue?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593166#M30342</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593167#M30343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 06 02:03:17 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Read this FAQ:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fbooting-lpc-link2" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Especially the Troubleshooting guide at the end.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593167#M30343</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso with LPC-Link2 jtag</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593168#M30344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aferrari on Thu Aug 06 07:03:00 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear Support,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks again for your help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the FAQ I've found the solution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem was a too long USB cable between the PC and the LPC-Link2 board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The cable is good because I normally use it with another debugger, but when I changed it with a shorter one everything started working fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Alberto&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-with-LPC-Link2-jtag/m-p/593168#M30344</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:31:50Z</dc:date>
    </item>
  </channel>
</rss>