<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Project Includes - Preprocessor Include Paths</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592868#M30202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Thu Jun 12 16:20:25 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, but my belief is that the Discovery Options are a v6.x setting and is not available in the v7.2&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I realize that the build is ok, it's just un-clean.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In v7 it seems to be Preprocessor Include Paths - I see them there, but can't get them to be active.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:48:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:48:46Z</dc:date>
    <item>
      <title>Project Includes - Preprocessor Include Paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592866#M30200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Thu Jun 12 11:42:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Win 7-64/LPCXpresso v7.2.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(Project)/Includes&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had created a project with two incorrect include paths for the _board and _chip paths. This causes a warning mark to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;be displayed (project exclamation point inside triangle icon), indicating that something is amiss, even after a correction. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking at the (Project)/Includes I see the two files that are greyed out as not resolved.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Checking the project &lt;/SPAN&gt;&lt;STRONG&gt;Preprocessor Include Paths, Macros etc.&lt;/STRONG&gt;&lt;SPAN&gt;, I see that the Debug build has two entries in &lt;/SPAN&gt;&lt;STRONG&gt;CDT Managed Setting Entries&lt;/STRONG&gt;&lt;SPAN&gt;, both of which describe the two non-existent files. However, the Action area (Add, Edit, Clear, Export) is also greyed out.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How can this be resolved short of a Delete/re-build of this Debug configuration?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592866#M30200</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: Project Includes - Preprocessor Include Paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592867#M30201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Thu Jun 12 13:23:32 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Finvalid-project-path-warnings" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/faq/lpcxpresso/invalid-project-path-warnings&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592867#M30201</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: Project Includes - Preprocessor Include Paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592868#M30202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Thu Jun 12 16:20:25 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, but my belief is that the Discovery Options are a v6.x setting and is not available in the v7.2&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I realize that the build is ok, it's just un-clean.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In v7 it seems to be Preprocessor Include Paths - I see them there, but can't get them to be active.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592868#M30202</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: Project Includes - Preprocessor Include Paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592869#M30203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 13 01:30:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, this did change in v7.2. However, a rebuild should clear the settings. Indeed, on the examples I have tried, these paths are reset. As I am unable to reproduce the problem, can you provide an example so that we can investigate?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592869#M30203</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: Project Includes - Preprocessor Include Paths</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592870#M30204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capstone on Mon Jun 16 16:51:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, but I did not see the notification for your response, and at the moment it seems I deleted &amp;amp; re-created that project since I couldn't clean.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will try to re-create, but this may have been caused by cut/paste with different projects. That practice has been found to create more problems that it's worth.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Project-Includes-Preprocessor-Include-Paths/m-p/592870#M30204</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:47Z</dc:date>
    </item>
  </channel>
</rss>