<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC-Link GDB command for Reset? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-GDB-command-for-Reset/m-p/592853#M30199</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bbolo1 on Tue Apr 02 00:16:48 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to debug some firmware that was made for LPC1114.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1114 is part of a bigger system in a power supply. On a particular board I have some issues and I need to capture the moment when some voltages are over a predefined threshold.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC-Link to debug this board however I am facing now a silly situation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What GDB command do I have to issue to reset the LPC1114?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen mentions on the web about "mon reset 8 -1 -1" but the GDB server ("crt_emu_lpc11_13_nxp.exe") seems not to support this command at all. :(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In contrast, whenever I am updating the firmware image, after the flashing process, the LPC1114 is reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The simple solution is to re-flash the firmware image all the time, but this doesn't seem like a nice solution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, the question is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone tell how to reset the MCU (issuing a GDB command) without having to re-flash?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mark&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:53:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:53:07Z</dc:date>
    <item>
      <title>LPC-Link GDB command for Reset?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-GDB-command-for-Reset/m-p/592853#M30199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bbolo1 on Tue Apr 02 00:16:48 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to debug some firmware that was made for LPC1114.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1114 is part of a bigger system in a power supply. On a particular board I have some issues and I need to capture the moment when some voltages are over a predefined threshold.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC-Link to debug this board however I am facing now a silly situation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What GDB command do I have to issue to reset the LPC1114?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen mentions on the web about "mon reset 8 -1 -1" but the GDB server ("crt_emu_lpc11_13_nxp.exe") seems not to support this command at all. :(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In contrast, whenever I am updating the firmware image, after the flashing process, the LPC1114 is reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The simple solution is to re-flash the firmware image all the time, but this doesn't seem like a nice solution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, the question is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone tell how to reset the MCU (issuing a GDB command) without having to re-flash?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mark&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Link-GDB-command-for-Reset/m-p/592853#M30199</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:07Z</dc:date>
    </item>
  </channel>
</rss>