<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 lpc18xx internal flash settings</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc18xx-internal-flash-settings/m-p/592546#M30052</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lalitshah233 on Sat Dec 15 21:26:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am new to NXP and LPC Xpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to know settings required in LPC xpresso to compile the System to run from internal flash memory of the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also i would like to know how to change this pointer for example i also need to compile the system in such a way that its base address would be &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;0x1a008000 instead of 0x1a000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried different settings, have used default settings but could not get success in it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Lalit Shah&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:30:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:30:18Z</dc:date>
    <item>
      <title>lpc18xx internal flash settings</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc18xx-internal-flash-settings/m-p/592546#M30052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lalitshah233 on Sat Dec 15 21:26:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am new to NXP and LPC Xpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to know settings required in LPC xpresso to compile the System to run from internal flash memory of the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also i would like to know how to change this pointer for example i also need to compile the system in such a way that its base address would be &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;0x1a008000 instead of 0x1a000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried different settings, have used default settings but could not get success in it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Lalit Shah&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpc18xx-internal-flash-settings/m-p/592546#M30052</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: lpc18xx internal flash settings</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpc18xx-internal-flash-settings/m-p/592547#M30053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Sun Dec 16 04:21:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When you create a project for an LPC18xx part with internal flash, such as LPC1857, then an appropriate flash driver will be automatically selected. For more information, please see the FAQ "LPC18xx/43xx Internal Flash Support" at:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/LPC18xx_43xx_InternalFlash&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[ Note that you do need to be using LPCXpresso v 4.30 or later to have access to this support.]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpc18xx-internal-flash-settings/m-p/592547#M30053</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:30:19Z</dc:date>
    </item>
  </channel>
</rss>