<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB_VBUS and ADC0_IN[4] - LPC178x in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-VBUS-and-ADC0-IN-4-LPC178x/m-p/592456#M30004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by graynomad on Wed Sep 14 08:10:56 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm designing a board based on the LPC178x, I need USB and all ADC inputs but there seems to be a clash between USB_VBUS and ADC0_IN[4] and neither can be moved to another pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Searching the web I cannot get a definitive answer as whether there is a work around or indeed if VBUS is really needed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual says&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;USB_VBUS &amp;amp;#8212; Monitors the presence of USB bus power.&lt;BR /&gt;This signal must be HIGH for USB reset to occur.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does this mean that once the chip (and USB) is booted I can use that pin for my ADC?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't believe they would assign two important functions to the pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;______&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:30:44 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:30:44Z</dc:date>
    <item>
      <title>USB_VBUS and ADC0_IN[4] - LPC178x</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-VBUS-and-ADC0-IN-4-LPC178x/m-p/592456#M30004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by graynomad on Wed Sep 14 08:10:56 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm designing a board based on the LPC178x, I need USB and all ADC inputs but there seems to be a clash between USB_VBUS and ADC0_IN[4] and neither can be moved to another pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Searching the web I cannot get a definitive answer as whether there is a work around or indeed if VBUS is really needed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual says&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;USB_VBUS &amp;amp;#8212; Monitors the presence of USB bus power.&lt;BR /&gt;This signal must be HIGH for USB reset to occur.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does this mean that once the chip (and USB) is booted I can use that pin for my ADC?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can't believe they would assign two important functions to the pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;______&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/USB-VBUS-and-ADC0-IN-4-LPC178x/m-p/592456#M30004</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:30:44Z</dc:date>
    </item>
  </channel>
</rss>