<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: NMI Interrupts</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/NMI-Interrupts/m-p/532225#M2973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by karanmehta93 on Sat Jan 19 14:17:49 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, The pin has multiple functions also. If not configured as input and NMI, by defaut it will work as a normal GPIO pin. And yes, Don't forget to put up external pull up on this pin.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 21:44:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T21:44:39Z</dc:date>
    <item>
      <title>NMI Interrupts</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/NMI-Interrupts/m-p/532224#M2972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sat Jan 19 05:49:03 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]If I never configure the pin (Port 2 pin 10 on an LPC1778) [/SIZE][/FONT][FONT=Tahoma][SIZE=1][SIZE=2]for NMI, is it true that an NMI interrupt can [I]never[/I] happen?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike[/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; [/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/NMI-Interrupts/m-p/532224#M2972</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: NMI Interrupts</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/NMI-Interrupts/m-p/532225#M2973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by karanmehta93 on Sat Jan 19 14:17:49 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, The pin has multiple functions also. If not configured as input and NMI, by defaut it will work as a normal GPIO pin. And yes, Don't forget to put up external pull up on this pin.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 21:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/NMI-Interrupts/m-p/532225#M2973</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T21:44:39Z</dc:date>
    </item>
  </channel>
</rss>