<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックWhat error is in the UART receive FIFO?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/What-error-is-in-the-UART-receive-FIFO/m-p/591386#M29566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sravet on Thu Oct 03 00:02:24 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working with UART2 on an LPC1768 part.&amp;nbsp; It is connected to an RF remote receiver that outputs data at 9600 baud.&amp;nbsp; I have configured UART2 for 9600 baud and verified that it works correctly by connecting it to my laptop via a USB/TTL serial converter.&amp;nbsp; Characters I type on the laptop are correctly received by the 1768.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However when I connect to the RF receiver I see constant line errors.&amp;nbsp; The LSR value I read is 0xe1.&amp;nbsp; This indicates RXFE (error in RX FIFO), Transmitter empty, and receiver data ready.&amp;nbsp; This doesn't make sense to me -- There is an error in the RX fifo, but none of the LSR error bits (break, parity, frame, overrun) are set.&amp;nbsp; What error is bit 7 indicating?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--steve&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:48:16 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:48:16Z</dc:date>
    <item>
      <title>What error is in the UART receive FIFO?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/What-error-is-in-the-UART-receive-FIFO/m-p/591386#M29566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sravet on Thu Oct 03 00:02:24 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working with UART2 on an LPC1768 part.&amp;nbsp; It is connected to an RF remote receiver that outputs data at 9600 baud.&amp;nbsp; I have configured UART2 for 9600 baud and verified that it works correctly by connecting it to my laptop via a USB/TTL serial converter.&amp;nbsp; Characters I type on the laptop are correctly received by the 1768.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However when I connect to the RF receiver I see constant line errors.&amp;nbsp; The LSR value I read is 0xe1.&amp;nbsp; This indicates RXFE (error in RX FIFO), Transmitter empty, and receiver data ready.&amp;nbsp; This doesn't make sense to me -- There is an error in the RX fifo, but none of the LSR error bits (break, parity, frame, overrun) are set.&amp;nbsp; What error is bit 7 indicating?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--steve&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:48:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/What-error-is-in-the-UART-receive-FIFO/m-p/591386#M29566</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:48:16Z</dc:date>
    </item>
  </channel>
</rss>