<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Strange Behaviour LPC11U37/401 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Strange-Behaviour-LPC11U37-401/m-p/590529#M29165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Apr 02 02:30:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What version of LPCXpresso are you using? You should be using v5.1.2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you still see problems with LPCXpresso v5.1.2, please can you post the full debug log:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/DebugLog&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would also be worth trying a mass erase before programming, to see if that cures the problem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/GuiFlashProgramming&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you also confirm if you see the same problem with all images, or just this particular one. For example if you create a "semihosting" project using the project wizard, do you see the same problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:53:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:53:23Z</dc:date>
    <item>
      <title>Strange Behaviour LPC11U37/401</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Strange-Behaviour-LPC11U37-401/m-p/590528#M29164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kemes on Mon Apr 01 11:12:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi to all &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am porting my code from LPC1114 to LPC11U37.&amp;nbsp; The code, that uses UART, compile and works well under LPC1114.&amp;nbsp; On the new processor the code compile correctly and works well except when I attempt to enable UART1.&amp;nbsp; In particular if I set :&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; LPC_IOCON-&amp;gt;PIO0_18 = 1;&amp;nbsp; // PIO0_18 is RXD&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; LPC_IOCON-&amp;gt;PIO0_19 = 1;&amp;nbsp; // PIO0_19 is RXD&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In order to config the usart1 pins, it compiles, but when I start debugging the result is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;15: Target error from Commit Flash write&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; Flash verify operation failed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And I can't debug.&amp;nbsp; if I comment the two lines, it compiles and downloads well (and, of course, doesn't work usart 1....) allowing me to debug.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There are some other settings ?&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Strange-Behaviour-LPC11U37-401/m-p/590528#M29164</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: Strange Behaviour LPC11U37/401</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Strange-Behaviour-LPC11U37-401/m-p/590529#M29165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Apr 02 02:30:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What version of LPCXpresso are you using? You should be using v5.1.2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you still see problems with LPCXpresso v5.1.2, please can you post the full debug log:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/DebugLog&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would also be worth trying a mass erase before programming, to see if that cures the problem:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/GuiFlashProgramming&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you also confirm if you see the same problem with all images, or just this particular one. For example if you create a "semihosting" project using the project wizard, do you see the same problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Strange-Behaviour-LPC11U37-401/m-p/590529#M29165</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:53:23Z</dc:date>
    </item>
  </channel>
</rss>